<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Anyone got Linux 3.1 or Linux 3.0 running on EVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167784#M4896</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you post your boot log?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2011 23:09:10 GMT</pubDate>
    <dc:creator>fabio_estevam</dc:creator>
    <dc:date>2011-09-02T23:09:10Z</dc:date>
    <item>
      <title>Anyone got Linux 3.1 or Linux 3.0 running on EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167783#M4895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have been trying for a day or so now to get the NFS booting of the Linux 3.x kernel. &amp;nbsp;There is a setting in there for the iMX28EVK but all we get is a hang once the kernel is starting up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have double checked the MACH_ID and that doesn't seem to be the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I'm just curious if anyone has this working.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;-steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 22:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167783#M4895</guid>
      <dc:creator>netstv</dc:creator>
      <dc:date>2011-09-02T22:21:55Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone got Linux 3.1 or Linux 3.0 running on EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167784#M4896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you post your boot log?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 23:09:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167784#M4896</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2011-09-02T23:09:10Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone got Linux 3.1 or Linux 3.0 running on EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167785#M4897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fabio,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I work with Steve. There is really nothing in the boot log. U-boot runs fine and loads the kernel, decompresses it and displays message "Starting kernel" and we don't see any console output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However when using 2.6.35 kernel and associated freescale patches, using the same u-boot and kernel command line parameters board boots just fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have noticed that there have been lot changes between 2.6.35 and the latest 3.1.0 RC available from ARM git and also 3.0 git source from pentronix git.&lt;/P&gt;&lt;P&gt;Particularly stuff in arch/arm/mx28, mx23 seems to have been consolidated into arch/arm/mach-mxs&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Sep 2011 10:46:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167785#M4897</guid>
      <dc:creator>SamGandhi</dc:creator>
      <dc:date>2011-09-03T10:46:06Z</dc:date>
    </item>
    <item>
      <title>Re: Anyone got Linux 3.1 or Linux 3.0 running on EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167786#M4898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;make sure that you have&lt;/P&gt;&lt;P&gt;CONFIG_SERIAL_AMBA_PL011=y&lt;BR /&gt;CONFIG_SERIAL_AMBA_PL011_CONSOLE=y&lt;/P&gt;&lt;P&gt;in Linux kernel config and your kernel command line looks like&lt;/P&gt;&lt;P&gt;console=&lt;STRONG&gt;ttyAMA0&lt;/STRONG&gt;,115200 root=/dev/mmcblk0p3 rw rootwait&lt;/P&gt;&lt;P&gt;you have to modify linux_prep bootlet to do so&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2011 05:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Anyone-got-Linux-3-1-or-Linux-3-0-running-on-EVK/m-p/167786#M4898</guid>
      <dc:creator>PavelNakonechny</dc:creator>
      <dc:date>2011-09-07T05:04:02Z</dc:date>
    </item>
  </channel>
</rss>