<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MMPF0100 I2C Programming in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-I2C-Programming/m-p/351789#M48929</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recently, I've received MMPF0100 parts with default configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to change some outputs to use them with my custom i.MX6 board. Specifically, I need &lt;/P&gt;&lt;P&gt;- 1.35V from SW3 instead of 1.5V default value&lt;/P&gt;&lt;P&gt;- 1.2V from SW4 instead of 1.8V default value&lt;/P&gt;&lt;P&gt;- 2.5V from VGEN4 instead of 1.8V default value&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And most importantly, I need these changes to be &lt;STRONG&gt;permanent&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am very confused about this issue. Do I need OTP feature in order to achieve this or can I do this on-board with just normal I2C operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jan 2015 12:37:51 GMT</pubDate>
    <dc:creator>durmus</dc:creator>
    <dc:date>2015-01-16T12:37:51Z</dc:date>
    <item>
      <title>MMPF0100 I2C Programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-I2C-Programming/m-p/351789#M48929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recently, I've received MMPF0100 parts with default configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to change some outputs to use them with my custom i.MX6 board. Specifically, I need &lt;/P&gt;&lt;P&gt;- 1.35V from SW3 instead of 1.5V default value&lt;/P&gt;&lt;P&gt;- 1.2V from SW4 instead of 1.8V default value&lt;/P&gt;&lt;P&gt;- 2.5V from VGEN4 instead of 1.8V default value&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And most importantly, I need these changes to be &lt;STRONG&gt;permanent&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am very confused about this issue. Do I need OTP feature in order to achieve this or can I do this on-board with just normal I2C operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 12:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-I2C-Programming/m-p/351789#M48929</guid>
      <dc:creator>durmus</dc:creator>
      <dc:date>2015-01-16T12:37:51Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0100 I2C Programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-I2C-Programming/m-p/351790#M48930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Durmuş&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to be permanent, OTP fuses should be programmed, programming script examples&lt;/P&gt;&lt;P&gt;can be found on link below.&lt;/P&gt;&lt;P&gt;Also voltages may be changed by I2C operation, after power-up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=KITPFGUI_4.0&amp;amp;location=null&amp;amp;Parent_nodeId=1339195063151733446987&amp;amp;Parent_pageType=product" title="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=KITPFGUI_4.0&amp;amp;location=null&amp;amp;Parent_nodeId=1339195063151733446987&amp;amp;Parent_pageType=product"&gt;KITPFGUI: GUI for the PF family development tools.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 14:57:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-I2C-Programming/m-p/351790#M48930</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-16T14:57:49Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0100 I2C Programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-I2C-Programming/m-p/351791#M48931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Durmus&lt;/P&gt;&lt;P&gt;In addition to what Igor suggests, to be able to&lt;/P&gt;&lt;P&gt;program the PMIC permanently, you need to &lt;/P&gt;&lt;P&gt;have the un-programmed version of the PMIC.&lt;/P&gt;&lt;P&gt;If you have a part that is preprogrammed you can&lt;/P&gt;&lt;P&gt;not change the values permanently. (Igor please&lt;/P&gt;&lt;P&gt;correct me if this is not correct).&lt;/P&gt;&lt;P&gt;A design alternative would be to have a preprogrammed&lt;/P&gt;&lt;P&gt;PMIC that mostly fits for the requirements and disable&lt;/P&gt;&lt;P&gt;the components that need different values. Then you&lt;/P&gt;&lt;P&gt;could change the values (e.g. SW3, SW4 and VGEN4&lt;/P&gt;&lt;P&gt;above) in your boot software. This way you can avoid&lt;/P&gt;&lt;P&gt;the additional process of programming your PMIC which&lt;/P&gt;&lt;P&gt;could make your manufacturing more complex.&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 15:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-I2C-Programming/m-p/351791#M48931</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2015-01-16T15:25:46Z</dc:date>
    </item>
  </channel>
</rss>