<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX53 QSB Ubuntu customisation, VPU problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167698#M4878</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I took the kernel which was tagged as Release in the git &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_2.6.35_11.09.01&amp;amp;id=691c08adeed64d5153937a0e31aaf4c251924471"&gt;(691c08adeed64d5153937a0e31aaf4c251924471)&lt;/A&gt; and applied the patches from the download section of the freescale website.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the hint with the new patch I'll update my kernel to the latest revision and will give it a try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Nov 2012 07:48:13 GMT</pubDate>
    <dc:creator>t_herbrecher</dc:creator>
    <dc:date>2012-11-12T07:48:13Z</dc:date>
    <item>
      <title>i.MX53 QSB Ubuntu customisation, VPU problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167695#M4875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello together,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we created a custom board with the i.MX537 for industrial applications. For test purposes we wanted to use the Ubuntu 10.04 Rootfilesystem to play a video via HDMI. The 1080p output via HDMI works perfect but when we want to play a video (the Sintel-Trailer.mp4 for example) causes an fatal error in the totem player, the gpu-sdk gui-example shows the videos as fat coloured stripes. Both explained test cases work on the QSB. We used the imx-2.6.35_11.09 tag of the freescale-git (uboot and kernel) plus the patches from the freescale download page for customization.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I have some questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Is there a difference between the i.MX535 processor used on the QSB and the i.MX537 on our board that could cause the described errors?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. When we load the described compiled kernel scources (git-tag plus patches) to the QSB and start to play a video on Ubuntu the IPU crashes with IPU_STATE5 and IPU_STATE10 error messages. Where is the difference of the kernel we compiled and the kernel used on the SD-card which is shipped with the QSB and the Ubuntu on it? Is the kernel source for the Ubuntu on the SD-card available out there or does anyone have the kernel-config used for this kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for your answers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2012 21:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167695#M4875</guid>
      <dc:creator>t_herbrecher</dc:creator>
      <dc:date>2012-11-07T21:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 QSB Ubuntu customisation, VPU problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167696#M4876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Timo,&lt;/P&gt;&lt;P&gt;I can help a little at least for 2.: zcat /proc/config.gz (by default, the built kernels provide the config used)&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2012 08:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167696#M4876</guid>
      <dc:creator>koobla</dc:creator>
      <dc:date>2012-11-09T08:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 QSB Ubuntu customisation, VPU problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167697#M4877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When did you take the kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using this kernel &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01"&gt;http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01&lt;/A&gt;&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure you have this patch: &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_2.6.35_11.09.01&amp;amp;id=bc8159027063aded47316b669b1293998337b2ee" style="color: #0000ff; text-decoration: underline; font-family: sans-serif; background-color: #eeeeee;"&gt;ENGR00230807 mxc v4l2 output:Use triple buffer for icbypass case&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2012 17:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167697#M4877</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2012-11-09T17:13:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 QSB Ubuntu customisation, VPU problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167698#M4878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I took the kernel which was tagged as Release in the git &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_2.6.35_11.09.01&amp;amp;id=691c08adeed64d5153937a0e31aaf4c251924471"&gt;(691c08adeed64d5153937a0e31aaf4c251924471)&lt;/A&gt; and applied the patches from the download section of the freescale website.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the hint with the new patch I'll update my kernel to the latest revision and will give it a try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2012 07:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167698#M4878</guid>
      <dc:creator>t_herbrecher</dc:creator>
      <dc:date>2012-11-12T07:48:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 QSB Ubuntu customisation, VPU problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167699#M4879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please, let us know the result.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2012 12:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-Ubuntu-customisation-VPU-problem/m-p/167699#M4879</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2012-11-12T12:19:38Z</dc:date>
    </item>
  </channel>
</rss>