<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Can pre-programed PMIC be replaced non-programed?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-pre-programed-PMIC-be-replaced-non-programed/m-p/350451#M48747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;AFAIK, NP types has to be programmed first. There is a&lt;/P&gt;&lt;P&gt;programmer reference circuitry from FSL you can&lt;/P&gt;&lt;P&gt;incorporate that into your design or program them before&lt;/P&gt;&lt;P&gt;you place them on your board. You can then later&lt;/P&gt;&lt;P&gt;modify the programmed values via I2C but the&lt;/P&gt;&lt;P&gt;changes are not permanent.&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Feb 2015 02:26:41 GMT</pubDate>
    <dc:creator>sinanakman</dc:creator>
    <dc:date>2015-02-05T02:26:41Z</dc:date>
    <item>
      <title>Can pre-programed PMIC be replaced non-programed?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-pre-programed-PMIC-be-replaced-non-programed/m-p/350450#M48746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been using &lt;SPAN lang="EN-US" style="color: #1f497d; font-family: '맑은 고딕'; font-size: 10pt; mso-bidi-font-family: 굴림; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA;"&gt;MMPF0100F1AEP, F1 type pre-programed PF0100, but our FSL distributor recomended &lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Arial','sans-serif'; font-size: 10pt; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA; mso-fareast-font-family: '맑은 고딕';"&gt;MMPF0200NPAEP, NON-programed PF0200.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: '맑은 고딕'; font-size: 10pt; mso-bidi-font-family: 굴림; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA;"&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Arial','sans-serif'; font-size: 10pt; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA; mso-fareast-font-family: '맑은 고딕';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: '맑은 고딕'; font-size: 10pt; mso-bidi-font-family: 굴림; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA;"&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Arial','sans-serif'; font-size: 10pt; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA; mso-fareast-font-family: '맑은 고딕';"&gt;The differences of PF0100 and PF0200 can be handled, but I am not sure F1 type can be replaced NP type.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: '맑은 고딕'; font-size: 10pt; mso-bidi-font-family: 굴림; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA;"&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Arial','sans-serif'; font-size: 10pt; mso-ansi-language: EN-US; mso-fareast-language: KO; mso-bidi-language: AR-SA; mso-fareast-font-family: '맑은 고딕';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Maybe programing for initial status will be needed to use NP type, is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is it possible to set PMIC in bootloader code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Feb 2015 01:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-pre-programed-PMIC-be-replaced-non-programed/m-p/350450#M48746</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-02-05T01:34:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can pre-programed PMIC be replaced non-programed?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-pre-programed-PMIC-be-replaced-non-programed/m-p/350451#M48747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;AFAIK, NP types has to be programmed first. There is a&lt;/P&gt;&lt;P&gt;programmer reference circuitry from FSL you can&lt;/P&gt;&lt;P&gt;incorporate that into your design or program them before&lt;/P&gt;&lt;P&gt;you place them on your board. You can then later&lt;/P&gt;&lt;P&gt;modify the programmed values via I2C but the&lt;/P&gt;&lt;P&gt;changes are not permanent.&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Feb 2015 02:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-pre-programed-PMIC-be-replaced-non-programed/m-p/350451#M48747</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2015-02-05T02:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: Can pre-programed PMIC be replaced non-programed?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-pre-programed-PMIC-be-replaced-non-programed/m-p/350452#M48748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; According to the MMPF0100 Datasheet, it "can be configured to start-up from either the internal OTP configuration, &lt;BR /&gt;or with a hard-coded configuration built in to the device. The internal hard-coded configuration is enabled by connecting &lt;BR /&gt;the VDDOTP pin to VCOREDIG through a 100 kohm resistor. The OTP configuration is enabled by connecting VDDOTP to GND.&lt;/P&gt;&lt;P&gt;For NP devices, selecting the OTP configuration causes the PF0100 to not start-up. However, the PF0100 can be controlled &lt;BR /&gt;through the I2C port for prototyping and programming. Once programmed, the NP device will startup with the customer programmed &lt;BR /&gt;configuration". &lt;BR /&gt;&amp;nbsp; So, for the NP devices, it is needed to use default hard-coded configuration. Please look at Table 10 (Start-up Configuration)&lt;BR /&gt;of the Datasheet for details.&lt;BR /&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: '맑은 고딕'; font-size: 10pt;"&gt; &lt;/SPAN&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Feb 2015 03:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-pre-programed-PMIC-be-replaced-non-programed/m-p/350452#M48748</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-02-05T03:56:24Z</dc:date>
    </item>
  </channel>
</rss>