<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDDR test failure with 2Gb RAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-test-failure-with-2Gb-RAM/m-p/350431#M48744</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;E:\soloX\Broad Bring up\DDR test\Sol SoloX larger RAM\DDR_Stress_Tester_V1.0.3_ENCORE\Binary&amp;gt;DDR_Stress_Tester.exe -t mx6x -df scripts\my.txt&lt;/P&gt;&lt;P&gt;MX6SX opened.&lt;/P&gt;&lt;P&gt;HAB_TYPE: DEVELOP&lt;/P&gt;&lt;P&gt;Image loading...&lt;/P&gt;&lt;P&gt;download Image to IRAM OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re-open MX6x device.&lt;/P&gt;&lt;P&gt;Running DDR test..., press "ESC" key to exit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;******************************&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR Stress Test (1.0.3) for MX6SX&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Build: Jun 25 2014, 12:09:14&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;******************************&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=======DDR configuration==========&lt;/P&gt;&lt;P&gt;DDR type is DDR3&lt;/P&gt;&lt;P&gt;Data width: 16, bank num: 8&lt;/P&gt;&lt;P&gt;Row size: 14, col size: 10&lt;/P&gt;&lt;P&gt;Chip select CSD0 is used&lt;/P&gt;&lt;P&gt;Density per chip select: 256MB&lt;/P&gt;&lt;P&gt;==================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What ARM core speed would you like to run?&lt;/P&gt;&lt;P&gt;Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz&lt;/P&gt;&lt;P&gt;&amp;nbsp; ARM set to 800MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please select the DDR density per chip select (in bytes) on the board&lt;/P&gt;&lt;P&gt;Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6&lt;/P&gt;&lt;P&gt;for 32MB&lt;/P&gt;&lt;P&gt;&amp;nbsp; DDR density selected (MB): 256&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Calibration will run at DDR frequency 400MHz. Type 'y' to continue.&lt;/P&gt;&lt;P&gt;If you want to run at other DDR frequency. Type 'n'&lt;/P&gt;&lt;P&gt;&amp;nbsp; DDR Freq: 396 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you like to run the write leveling calibration? (y/n)&lt;/P&gt;&lt;P&gt;&amp;nbsp; You have chosen not to run the write level calibration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you like to run the DQS gating, read/write delay calibration? (y/n)&lt;/P&gt;&lt;P&gt;Starting DQS gating calibration...&lt;/P&gt;&lt;P&gt;. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!&lt;/P&gt;&lt;P&gt;dram test fails for all values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DDR stress test can run with an incrementing frequency or at a static freq&lt;/P&gt;&lt;P&gt;To run at a static freq, simply set the start freq and end freq to the same valu&lt;/P&gt;&lt;P&gt;e&lt;/P&gt;&lt;P&gt;Would you like to run the DDR Stress Test (y/n)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Nov 2014 17:59:42 GMT</pubDate>
    <dc:creator>liangchai</dc:creator>
    <dc:date>2014-11-18T17:59:42Z</dc:date>
    <item>
      <title>DDR test failure with 2Gb RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-test-failure-with-2Gb-RAM/m-p/350431#M48744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;E:\soloX\Broad Bring up\DDR test\Sol SoloX larger RAM\DDR_Stress_Tester_V1.0.3_ENCORE\Binary&amp;gt;DDR_Stress_Tester.exe -t mx6x -df scripts\my.txt&lt;/P&gt;&lt;P&gt;MX6SX opened.&lt;/P&gt;&lt;P&gt;HAB_TYPE: DEVELOP&lt;/P&gt;&lt;P&gt;Image loading...&lt;/P&gt;&lt;P&gt;download Image to IRAM OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re-open MX6x device.&lt;/P&gt;&lt;P&gt;Running DDR test..., press "ESC" key to exit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;******************************&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR Stress Test (1.0.3) for MX6SX&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Build: Jun 25 2014, 12:09:14&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;******************************&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=======DDR configuration==========&lt;/P&gt;&lt;P&gt;DDR type is DDR3&lt;/P&gt;&lt;P&gt;Data width: 16, bank num: 8&lt;/P&gt;&lt;P&gt;Row size: 14, col size: 10&lt;/P&gt;&lt;P&gt;Chip select CSD0 is used&lt;/P&gt;&lt;P&gt;Density per chip select: 256MB&lt;/P&gt;&lt;P&gt;==================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What ARM core speed would you like to run?&lt;/P&gt;&lt;P&gt;Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz&lt;/P&gt;&lt;P&gt;&amp;nbsp; ARM set to 800MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please select the DDR density per chip select (in bytes) on the board&lt;/P&gt;&lt;P&gt;Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6&lt;/P&gt;&lt;P&gt;for 32MB&lt;/P&gt;&lt;P&gt;&amp;nbsp; DDR density selected (MB): 256&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Calibration will run at DDR frequency 400MHz. Type 'y' to continue.&lt;/P&gt;&lt;P&gt;If you want to run at other DDR frequency. Type 'n'&lt;/P&gt;&lt;P&gt;&amp;nbsp; DDR Freq: 396 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you like to run the write leveling calibration? (y/n)&lt;/P&gt;&lt;P&gt;&amp;nbsp; You have chosen not to run the write level calibration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you like to run the DQS gating, read/write delay calibration? (y/n)&lt;/P&gt;&lt;P&gt;Starting DQS gating calibration...&lt;/P&gt;&lt;P&gt;. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!&lt;/P&gt;&lt;P&gt;dram test fails for all values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DDR stress test can run with an incrementing frequency or at a static freq&lt;/P&gt;&lt;P&gt;To run at a static freq, simply set the start freq and end freq to the same valu&lt;/P&gt;&lt;P&gt;e&lt;/P&gt;&lt;P&gt;Would you like to run the DDR Stress Test (y/n)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 17:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-test-failure-with-2Gb-RAM/m-p/350431#M48744</guid>
      <dc:creator>liangchai</dc:creator>
      <dc:date>2014-11-18T17:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: DDR test failure with 2Gb RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-test-failure-with-2Gb-RAM/m-p/350432#M48745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Liang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can check common guidelines&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101708"&gt;Freescale i.MX6 DRAM Port Application Guide-DDR3&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding "DQS gating calibration.... . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!"&lt;/P&gt;&lt;P&gt;first time you can just ignore it and continue to run remaining tests, just check if they will work.&lt;/P&gt;&lt;P&gt;This error is caused by excessive board noise, one can try to play with&lt;/P&gt;&lt;P&gt;drive strength settings (both i.MX6 and DDR memory), try different DDR_SEL options, use WALAT=1&lt;/P&gt;&lt;P&gt;and decrease operating frequency as much as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Nov 2014 11:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-test-failure-with-2Gb-RAM/m-p/350432#M48745</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-11-19T11:10:46Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-test-failure-with-2Gb-RAM/m-p/1136045#M161133</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 15:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-test-failure-with-2Gb-RAM/m-p/1136045#M161133</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T15:07:51Z</dc:date>
    </item>
  </channel>
</rss>