<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HAB events when using imx_usb_loader in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HAB-events-when-using-imx-usb-loader/m-p/349965#M48598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load my image from SPI-NOR I don't get HAB events.&lt;/P&gt;&lt;P&gt;If I switch to the serial loader boot mode and load the same image I get HAB events.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I compare the RAM data of the working u-boot image with the non-working image I see the imx_usb_loader version has its IVT dcd and boot_data fields cleared.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;working:&lt;/P&gt;&lt;P&gt;177ff400: d1 00 20 40 00 00 80 17 00 00 00 00 2c f4 7f 17&amp;nbsp;&amp;nbsp;&amp;nbsp; .. @........,...&lt;/P&gt;&lt;P&gt;177ff410: 20 f4 7f 17 00 f4 7f 17 00 10 86 17 00 00 00 00&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ...............&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;non working:&lt;/P&gt;&lt;P&gt;177ff400: d1 00 20 40 00 00 80 17 00 00 00 00 00 00 00 00&amp;nbsp;&amp;nbsp;&amp;nbsp; .. @............&lt;/P&gt;&lt;P&gt;177ff410: 00 00 00 00 00 f4 7f 17 00 10 86 17 00 00 00 00&amp;nbsp;&amp;nbsp;&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody experienced this issue? Has anybody worked around this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using imx_usb_loader master branch f96aee286ea17c832b7ec922dd76842deb5ce299 and a nitrogen6x development board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jan 2015 00:06:44 GMT</pubDate>
    <dc:creator>andrelabelle</dc:creator>
    <dc:date>2015-01-16T00:06:44Z</dc:date>
    <item>
      <title>HAB events when using imx_usb_loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-events-when-using-imx-usb-loader/m-p/349965#M48598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load my image from SPI-NOR I don't get HAB events.&lt;/P&gt;&lt;P&gt;If I switch to the serial loader boot mode and load the same image I get HAB events.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I compare the RAM data of the working u-boot image with the non-working image I see the imx_usb_loader version has its IVT dcd and boot_data fields cleared.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;working:&lt;/P&gt;&lt;P&gt;177ff400: d1 00 20 40 00 00 80 17 00 00 00 00 2c f4 7f 17&amp;nbsp;&amp;nbsp;&amp;nbsp; .. @........,...&lt;/P&gt;&lt;P&gt;177ff410: 20 f4 7f 17 00 f4 7f 17 00 10 86 17 00 00 00 00&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ...............&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;non working:&lt;/P&gt;&lt;P&gt;177ff400: d1 00 20 40 00 00 80 17 00 00 00 00 00 00 00 00&amp;nbsp;&amp;nbsp;&amp;nbsp; .. @............&lt;/P&gt;&lt;P&gt;177ff410: 00 00 00 00 00 f4 7f 17 00 10 86 17 00 00 00 00&amp;nbsp;&amp;nbsp;&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody experienced this issue? Has anybody worked around this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using imx_usb_loader master branch f96aee286ea17c832b7ec922dd76842deb5ce299 and a nitrogen6x development board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 00:06:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-events-when-using-imx-usb-loader/m-p/349965#M48598</guid>
      <dc:creator>andrelabelle</dc:creator>
      <dc:date>2015-01-16T00:06:44Z</dc:date>
    </item>
    <item>
      <title>Re: HAB events when using imx_usb_loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-events-when-using-imx-usb-loader/m-p/349966#M48599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please refer to section 6.2 (Signing Code Downloadable with Manufacturing Tool) of app note&lt;BR /&gt;AN4581 (&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4&lt;/SPAN&gt;) &lt;BR /&gt;regarding specifics of using the i.MX6 Serial (USB) Downloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 05:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-events-when-using-imx-usb-loader/m-p/349966#M48599</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-01-20T05:52:44Z</dc:date>
    </item>
  </channel>
</rss>