<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックI2C Bus test</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I2C-Bus-test/m-p/349928#M48576</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i try to test the I2C Bus of IMX6 automotive.&lt;/P&gt;&lt;P&gt;with the command i2cdetect -l,the microcontroller has 2 bus (1 and 2).&lt;/P&gt;&lt;P&gt;with the command i2cdetect 1 ,i have one sensor on 0x48&lt;/P&gt;&lt;P&gt;i see to the datensheet that 0x90 is the chip address to Read/Writte&lt;/P&gt;&lt;P&gt;now i wan to read and writte&lt;/P&gt;&lt;P&gt;i use the command i2cget 1 0x48 0x90&lt;/P&gt;&lt;P&gt;but the answer is read failed.&lt;/P&gt;&lt;P&gt;Please why can i do ,to have some answer ?&lt;/P&gt;&lt;P&gt;and why can i don to writte with the command i2cset?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Sep 2014 11:09:20 GMT</pubDate>
    <dc:creator>yannkingoum</dc:creator>
    <dc:date>2014-09-09T11:09:20Z</dc:date>
    <item>
      <title>I2C Bus test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-Bus-test/m-p/349928#M48576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i try to test the I2C Bus of IMX6 automotive.&lt;/P&gt;&lt;P&gt;with the command i2cdetect -l,the microcontroller has 2 bus (1 and 2).&lt;/P&gt;&lt;P&gt;with the command i2cdetect 1 ,i have one sensor on 0x48&lt;/P&gt;&lt;P&gt;i see to the datensheet that 0x90 is the chip address to Read/Writte&lt;/P&gt;&lt;P&gt;now i wan to read and writte&lt;/P&gt;&lt;P&gt;i use the command i2cget 1 0x48 0x90&lt;/P&gt;&lt;P&gt;but the answer is read failed.&lt;/P&gt;&lt;P&gt;Please why can i do ,to have some answer ?&lt;/P&gt;&lt;P&gt;and why can i don to writte with the command i2cset?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 11:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-Bus-test/m-p/349928#M48576</guid>
      <dc:creator>yannkingoum</dc:creator>
      <dc:date>2014-09-09T11:09:20Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Bus test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-Bus-test/m-p/349929#M48577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have problems when using i2cdump too?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Sep 2014 15:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-Bus-test/m-p/349929#M48577</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-09-11T15:43:58Z</dc:date>
    </item>
  </channel>
</rss>