<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 SABRESD Red Led no boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349838#M48546</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrea&lt;/P&gt;&lt;P&gt;The SPI is normally not populated on an sabresd board if this&lt;/P&gt;&lt;P&gt;is what you referring to.&amp;nbsp; You can build a u-boot image and&lt;/P&gt;&lt;P&gt;boot your board from SD. If you have a JTAG tool, try to&lt;/P&gt;&lt;P&gt;halt after reset and check if you can read part of ram to make&lt;/P&gt;&lt;P&gt;sure your board is alive. I am not sure which red light you&lt;/P&gt;&lt;P&gt;are referring to. Perhaps you can check in its user guide to&lt;/P&gt;&lt;P&gt;see what a red led is indicating.&lt;/P&gt;&lt;P&gt;In either way, if your board is still alive, build an u-boot image&lt;/P&gt;&lt;P&gt;for your board and place it to an sd card as explained in&lt;/P&gt;&lt;P&gt;several places in this forum. Then you will be able to boot&lt;/P&gt;&lt;P&gt;your u-boot and you can continue loading a Linux image.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Sep 2014 14:38:53 GMT</pubDate>
    <dc:creator>sinanakman</dc:creator>
    <dc:date>2014-09-26T14:38:53Z</dc:date>
    <item>
      <title>IMX6 SABRESD Red Led no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349837#M48545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a Freescale IMX6 SabreSD Board with a iMX6 Quad Processor.&lt;/P&gt;&lt;P&gt;Until this morning everything was working fine.&lt;/P&gt;&lt;P&gt;The board was booting Yocto Linux from a SD Card.&lt;/P&gt;&lt;P&gt;I have removed all kernel modules with the command: rmmod *&lt;/P&gt;&lt;P&gt;After reboot the red led is permanently ON.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did I corrupted the internal flash ?&lt;/P&gt;&lt;P&gt;How to find the flash image to upload via JTAG (if possible) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Andrea&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 13:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349837#M48545</guid>
      <dc:creator>andreatessadri</dc:creator>
      <dc:date>2014-09-26T13:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 SABRESD Red Led no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349838#M48546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrea&lt;/P&gt;&lt;P&gt;The SPI is normally not populated on an sabresd board if this&lt;/P&gt;&lt;P&gt;is what you referring to.&amp;nbsp; You can build a u-boot image and&lt;/P&gt;&lt;P&gt;boot your board from SD. If you have a JTAG tool, try to&lt;/P&gt;&lt;P&gt;halt after reset and check if you can read part of ram to make&lt;/P&gt;&lt;P&gt;sure your board is alive. I am not sure which red light you&lt;/P&gt;&lt;P&gt;are referring to. Perhaps you can check in its user guide to&lt;/P&gt;&lt;P&gt;see what a red led is indicating.&lt;/P&gt;&lt;P&gt;In either way, if your board is still alive, build an u-boot image&lt;/P&gt;&lt;P&gt;for your board and place it to an sd card as explained in&lt;/P&gt;&lt;P&gt;several places in this forum. Then you will be able to boot&lt;/P&gt;&lt;P&gt;your u-boot and you can continue loading a Linux image.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 14:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349838#M48546</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2014-09-26T14:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 SABRESD Red Led no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349839#M48547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sinan,&lt;/P&gt;&lt;P&gt;&amp;nbsp; the red led is the D3 between the power connector and the SIM card slot.&lt;/P&gt;&lt;P&gt;I don't have a JTAG but I have successfully performed the download of the factory firmware with MFGtool.&lt;/P&gt;&lt;P&gt;Unfortunately the board still cannot boot.&lt;/P&gt;&lt;P&gt;Any suggestion is very welcomed.&lt;/P&gt;&lt;P&gt;Looking forward&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Andrea&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 15:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349839#M48547</guid>
      <dc:creator>andreatessadri</dc:creator>
      <dc:date>2014-09-26T15:28:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 SABRESD Red Led no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349840#M48548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrea, D3 is red while I am at u-boot in my board as well. This should be no problem.&lt;/P&gt;&lt;P&gt;I am not familiar with MFGTool and as mentioned my best suggestion would be&amp;nbsp; to build an uboot&lt;/P&gt;&lt;P&gt;image and place it on SD then boot it from SD. I know this works if your board is fine.&lt;/P&gt;&lt;P&gt;Also, our sabred came with a preloaded SD card that you can boot uboot. If you still have this&lt;/P&gt;&lt;P&gt;original SD you can boot into uboot and you can then boot kernel from there.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 15:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SABRESD-Red-Led-no-boot/m-p/349840#M48548</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2014-09-26T15:45:43Z</dc:date>
    </item>
  </channel>
</rss>