<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Does Android JB supports Dual Display? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-Android-JB-supports-Dual-Display/m-p/349394#M48461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I have a custom iMX6-solo board and am trying dual display on two LVDS showing different contents. Though LVDS can be operated in four modes namely split,dual,separate and single, I could get only mirror image of one lvds display over the other. Does Android OS recognizes two displays at a time ? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 14 Dec 2014 14:05:10 GMT</pubDate>
    <dc:creator>teddy123</dc:creator>
    <dc:date>2014-12-14T14:05:10Z</dc:date>
    <item>
      <title>Does Android JB supports Dual Display?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Android-JB-supports-Dual-Display/m-p/349394#M48461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I have a custom iMX6-solo board and am trying dual display on two LVDS showing different contents. Though LVDS can be operated in four modes namely split,dual,separate and single, I could get only mirror image of one lvds display over the other. Does Android OS recognizes two displays at a time ? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Dec 2014 14:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Android-JB-supports-Dual-Display/m-p/349394#M48461</guid>
      <dc:creator>teddy123</dc:creator>
      <dc:date>2014-12-14T14:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: Does Android JB supports Dual Display?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Android-JB-supports-Dual-Display/m-p/349395#M48462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Teddy123，&lt;/P&gt;&lt;P&gt;Which version of android BSP are you using? android_jb4.2.2_1.1.0-ga_source or android_jb4.3_1.0.0-ga_source?&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 01:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Android-JB-supports-Dual-Display/m-p/349395#M48462</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-12-15T01:39:16Z</dc:date>
    </item>
    <item>
      <title>Re: Does Android JB supports Dual Display?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Android-JB-supports-Dual-Display/m-p/349396#M48463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;teddy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Android Doesn't provide this feature.&lt;/P&gt;&lt;P&gt;You need to modified the Android frame works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have specific content needs to run on 2nd display than it can be possible with minimal change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 04:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Android-JB-supports-Dual-Display/m-p/349396#M48463</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-12-15T04:47:43Z</dc:date>
    </item>
  </channel>
</rss>