<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6SL GPIO Interrupt latency (Yocto Project) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-GPIO-Interrupt-latency-Yocto-Project/m-p/349084#M48395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Induk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;since linux is not real time OS such time is normal,&lt;/P&gt;&lt;P&gt;you can refer to below context latencies (interrupts use&lt;/P&gt;&lt;P&gt;this context switching)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Context switching - times in microseconds&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94571"&gt;LMbench Benchmarks on i.MX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Sep 2014 08:02:45 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-09-26T08:02:45Z</dc:date>
    <item>
      <title>iMX6SL GPIO Interrupt latency (Yocto Project)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-GPIO-Interrupt-latency-Yocto-Project/m-p/349083#M48394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the GPIO Interrupt, but the interrupt response time is too long (20us more)&lt;/P&gt;&lt;P&gt;How do you feel about the following statements?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;iMX6SL, Yocto Project, linux kenel 3.10.17&lt;/P&gt;&lt;P&gt;Please help me......&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gpio_request(97,"test1"); //GPIO4 1 Intertup source&lt;/P&gt;&lt;P&gt;gpio_request(26,"test2"); //GPIO0 26 Out Control&lt;/P&gt;&lt;P&gt;gpio_direction_input(97);&lt;/P&gt;&lt;P&gt;gpio_direction_output(26,0);&lt;/P&gt;&lt;P&gt;int irq = gpio_to_irq(97);&lt;/P&gt;&lt;P&gt;int ret = request_irq(irq,test_isr,IRQF_TRIGGER_FALLING|IRQF_TRIGGER_RISING, "gpiodev", NULL);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;irqreturn_t test_isr(int irq, void *dev_id)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; gpio_set_value(26,1);&lt;/P&gt;&lt;P&gt;&amp;nbsp; gpio_set_value(26,0);&lt;/P&gt;&lt;P&gt;&amp;nbsp; gpio_set_value(26,1);&lt;/P&gt;&lt;P&gt;&amp;nbsp; gpio_set_value(26,0);&lt;/P&gt;&lt;P&gt;&amp;nbsp; return IRQ_HANDLED;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="scope_5.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46265i914AC47EB087B951/image-size/large?v=v2&amp;amp;px=999" role="button" title="scope_5.bmp" alt="scope_5.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 06:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-GPIO-Interrupt-latency-Yocto-Project/m-p/349083#M48394</guid>
      <dc:creator>indukkim</dc:creator>
      <dc:date>2014-09-26T06:21:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SL GPIO Interrupt latency (Yocto Project)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-GPIO-Interrupt-latency-Yocto-Project/m-p/349084#M48395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Induk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;since linux is not real time OS such time is normal,&lt;/P&gt;&lt;P&gt;you can refer to below context latencies (interrupts use&lt;/P&gt;&lt;P&gt;this context switching)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Context switching - times in microseconds&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94571"&gt;LMbench Benchmarks on i.MX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 08:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-GPIO-Interrupt-latency-Yocto-Project/m-p/349084#M48395</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-26T08:02:45Z</dc:date>
    </item>
  </channel>
</rss>