<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Limit USB speed on imx6dl</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348602#M48296</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to implement the patch but at the moment looks dosen't works.&lt;/P&gt;&lt;P&gt;Still, if I plug in USB-stick it gets identified as high speed device and not full speed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that the function hw_device_reset(struct ci_hdrc *ci, u32 mode) where I implement&lt;/P&gt;&lt;P&gt;the patch is never executed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shuld works also with Host H1 controller or only with OTG?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Mar 2015 15:46:48 GMT</pubDate>
    <dc:creator>guidopalmieri</dc:creator>
    <dc:date>2015-03-02T15:46:48Z</dc:date>
    <item>
      <title>Limit USB speed on imx6dl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348600#M48294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using imx6dl and kernel 3.10.17.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to limit the USB speed of the my H1 USB-controller to Full-Speed (USB1) even when&amp;nbsp; it is connect to a USB device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that in mainline is needed to set the PFSC bit into PORTSC register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea to do that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 09:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348600#M48294</guid>
      <dc:creator>guidopalmieri</dc:creator>
      <dc:date>2015-03-02T09:47:06Z</dc:date>
    </item>
    <item>
      <title>Re: Limit USB speed on imx6dl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348601#M48295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guido&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at below link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="337237" data-objecttype="1" href="https://community.freescale.com/thread/337237"&gt;https://community.freescale.com/thread/337237&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 11:53:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348601#M48295</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-02T11:53:16Z</dc:date>
    </item>
    <item>
      <title>Re: Limit USB speed on imx6dl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348602#M48296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to implement the patch but at the moment looks dosen't works.&lt;/P&gt;&lt;P&gt;Still, if I plug in USB-stick it gets identified as high speed device and not full speed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that the function hw_device_reset(struct ci_hdrc *ci, u32 mode) where I implement&lt;/P&gt;&lt;P&gt;the patch is never executed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shuld works also with Host H1 controller or only with OTG?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 15:46:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348602#M48296</guid>
      <dc:creator>guidopalmieri</dc:creator>
      <dc:date>2015-03-02T15:46:48Z</dc:date>
    </item>
    <item>
      <title>Re: Limit USB speed on imx6dl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348603#M48297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guido,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe you can reference this patch from mainline:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;commit 4f6743d5ca97ac66831add302cc546&lt;/P&gt;&lt;P class="a3s"&gt;7db4ee3809&lt;BR /&gt; Author: Michael Grzeschik &amp;lt;&lt;A href="mailto:m.grzeschik@pengutronix.de"&gt;m.grzeschik@pengutronix.de&lt;/A&gt;&amp;gt;&lt;BR /&gt; Date:&amp;nbsp;&amp;nbsp; Wed Feb 19 13:41:43 2014 +0800&lt;BR /&gt; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; usb: chipidea: udc: add maximum-speed = full-speed option&lt;BR /&gt; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This patch makes it possible to set the chipidea udc into full-speed only mo&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It is set by the oftree property "maximum-speed = full-speed".&lt;BR /&gt; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Signed-off-by: Peter Chen &amp;lt;&lt;A href="mailto:peter.chen@freescale.com"&gt;peter.chen@freescale.com&lt;/A&gt;&amp;gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Signed-off-by: Michael Grzeschik &amp;lt;&lt;A href="mailto:m.grzeschik@pengutronix.de"&gt;m.grzeschik@pengutronix.de&lt;/A&gt;&amp;gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Signed-off-by: Marc Kleine-Budde &amp;lt;&lt;A href="mailto:mkl@pengutronix.de"&gt;mkl@pengutronix.de&lt;/A&gt;&amp;gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Signed-off-by: Greg Kroah-Hartman &amp;lt;&lt;A href="mailto:gregkh@linuxfoundation.org"&gt;gregkh@linuxfoundation.org&lt;/A&gt;&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 18:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Limit-USB-speed-on-imx6dl/m-p/348603#M48297</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-03-02T18:03:52Z</dc:date>
    </item>
  </channel>
</rss>