<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Error while before boot script on Saber Lite 6Q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347616#M48127</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the I2C lines if it is shorted with the GND pin in the J7. Also checked with reference to some of the common GND points on the boards,&lt;/P&gt;&lt;P&gt;but it seems there is no shorting there. Can you suggest any other point in particular which should be checked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also checked the pull-up registers for these pins r216 and r217. They seem fine, i mean measures the correct resistance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Anil Ghadiya &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Dec 2014 07:34:30 GMT</pubDate>
    <dc:creator>anilghadiya</dc:creator>
    <dc:date>2014-12-01T07:34:30Z</dc:date>
    <item>
      <title>Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347611#M48122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are getting error while booting the IMX Saberlite 6Q from SD card.&lt;/P&gt;&lt;P&gt;Below is the error log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.2 at 792 MHz&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: SABRE Lite&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 1 GiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/P&gt;&lt;P&gt;SF: Detected SST25VF016B with page size 4 KiB, total 2 MiB&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x4 retry=0&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x4 retry=1&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x4 retry=2&lt;/P&gt;&lt;P&gt;i2c_init_transfer: give up i2c_regs=021a8000&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x38 retry=0&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x38 retry=1&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x38 retry=2&lt;/P&gt;&lt;P&gt;i2c_init_transfer: give up i2c_regs=021a8000&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x48 retry=0&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x48 retry=1&lt;/P&gt;&lt;P&gt;wait_for_sr_state: failed sr=81 cr=a0 state=2020&lt;/P&gt;&lt;P&gt;i2c_init_transfer: failed for chip 0x48 retry=2&lt;/P&gt;&lt;P&gt;i2c_init_transfer: give up i2c_regs=021a8000&lt;/P&gt;&lt;P&gt;No panel detected: default to HDMI&lt;/P&gt;&lt;P&gt;enable_hdmi: setup HDMI monitor&lt;/P&gt;&lt;P&gt;Display: HDMI (1024x768)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; using phy at 6&lt;/P&gt;&lt;P&gt;FEC [PRIME]&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;/P&gt;&lt;P&gt;flags: ncq stag pm led clo only pmp pio slum part&lt;/P&gt;&lt;P&gt;No port device detected!&lt;/P&gt;&lt;P&gt;** Bad device size - sata 0 **&lt;/P&gt;&lt;P&gt;** Bad device size - sata 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SATA device 1: unknown device&lt;/P&gt;&lt;P&gt;** Bad device sata 1 **&lt;/P&gt;&lt;P&gt;** Bad device sata 1 **&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;/P&gt;&lt;P&gt;mmc0(part 0) is current device&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;/P&gt;&lt;P&gt;** Bad device mmc 0 **&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;/P&gt;&lt;P&gt;** Bad device mmc 0 **&lt;/P&gt;&lt;P&gt;mmc1 is current device&lt;/P&gt;&lt;P&gt;** Unrecognized filesystem type **&lt;/P&gt;&lt;P&gt;1653 bytes read in 59 ms (27.3 KiB/s)&lt;/P&gt;&lt;P&gt;## Executing script at 10008000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We changed the kernel image and try but it gives the same error. We are using Kernel 3.0.35.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Anil Ghadiya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 07:11:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347611#M48122</guid>
      <dc:creator>anilghadiya</dc:creator>
      <dc:date>2014-11-18T07:11:23Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347612#M48123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These errors indicate that something is holding the I2C bus in an invalid state and come from the attempt to auto-detect displays through their touch controllers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you have connected to the board (especially J7)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 13:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347612#M48123</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-11-18T13:43:11Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347613#M48124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have connected our device via I2C to J7 (Only I2C pins and GPIO_9) and we are using this setup since beginning.&lt;/P&gt;&lt;P&gt;This issue started once after the application caused the kernel panic. So we suspected that flash is corrupted and tried to&lt;/P&gt;&lt;P&gt;re-flash it from SD card. But we are not able to flash it again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be very helpful if you can guide us to re-flash the SPI_NOR in such a way that it boots up from micro SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Anil Ghadiya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 17:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347613#M48124</guid>
      <dc:creator>anilghadiya</dc:creator>
      <dc:date>2014-11-18T17:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347614#M48125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are able re-flash the board and its booting up but it gives the same errors which i mentioned in the first post.&lt;/P&gt;&lt;P&gt;As i mentioned we are connecting our device to J7(Only I2C pins and GPIO_9) via I2C.&lt;/P&gt;&lt;P&gt;Even if do not connect anything on J7, we are getting the same error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Anil Ghadiya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Nov 2014 13:52:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347614#M48125</guid>
      <dc:creator>anilghadiya</dc:creator>
      <dc:date>2014-11-27T13:52:30Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347615#M48126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;These I2C error messages indicate that something is holding the I2C lines (SDA and/or SCL) low (holding the I2C bus).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you've disconnected your device, perhaps the process introduces a short to ground somewhere.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Nov 2014 18:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347615#M48126</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-11-30T18:59:53Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347616#M48127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the I2C lines if it is shorted with the GND pin in the J7. Also checked with reference to some of the common GND points on the boards,&lt;/P&gt;&lt;P&gt;but it seems there is no shorting there. Can you suggest any other point in particular which should be checked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also checked the pull-up registers for these pins r216 and r217. They seem fine, i mean measures the correct resistance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Anil Ghadiya &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 07:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347616#M48127</guid>
      <dc:creator>anilghadiya</dc:creator>
      <dc:date>2014-12-01T07:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347617#M48128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you set the SION bits in the MUX_CTL_PAD registers, you can validate that the pins are reading low&lt;/P&gt;&lt;P&gt;in the GPIOx_PSR registers (GP1:5 and GP7:11):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="https://github.com/boundarydevices/u-boot-imx6/blob/production/board/boundary/nitrogen6x/nitrogen6x.c#L123" title="https://github.com/boundarydevices/u-boot-imx6/blob/production/board/boundary/nitrogen6x/nitrogen6x.c#L123"&gt;https://github.com/boundarydevices/u-boot-imx6/blob/production/board/boundary/nitrogen6x/nitrogen6x.c#L123&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use the "mm.l" command in U-Boot to view/change the register values.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 17:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347617#M48128</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-12-01T17:26:04Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347618#M48129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have tried to read the MUX_CTL_PAD and GPIOx_PSR registers from the u-boot prompt.&lt;/P&gt;&lt;P&gt;But we are getting the same values for all registers.&lt;/P&gt;&lt;P&gt;Could you please take a look and check if we are reading it correctly and what do the read values indicate?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48265i7B79794E8A3423C1/image-size/large?v=v2&amp;amp;px=999" title="ReadValues.jpg" alt="ReadValues.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance,&lt;/P&gt;&lt;P&gt;Anil Ghadiya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 11:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347618#M48129</guid>
      <dc:creator>anilghadiya</dc:creator>
      <dc:date>2014-12-15T11:47:43Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347619#M48130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The &lt;TT&gt;mm.l&lt;/TT&gt; command expects an address as its argument. You can find the addresses in the &lt;SPAN style="font-size: 13.6000003814697px;"&gt;reference manual &lt;/SPAN&gt;i.MX6DQRM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 14:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347619#M48130</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-12-15T14:49:18Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347620#M48131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have read the below mentioned registers.....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. IOMUXC_SW_MUX_CTL_PAD_EIM_DATA17 @ addr 0x20E0094&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;2. IOMUXC_SW_MUX_CTL_PAD_EIM_DATA18 @ addr 0x20E0098&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;3. IOMUXC_I2C3_SCL_IN_SELECT_INPUT @ addr 0x20E08A8&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;4. IOMUXC_I2C3_SDA_IN_SELECT_INPUT &lt;SPAN style="font-size: 13.63636302948px;"&gt;@ addr 0x20E08AC&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;5. GPIO1_PSR @ addr 0x209C008&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;6. GPIO7_PSR @ addr 0x20B4008&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;Could you please take a look at the read values and see if anything is missing.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;Please see the image for corresponding read values.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48394iF4D90983C95C8D90/image-size/large?v=v2&amp;amp;px=999" title="imx.jpg" alt="imx.jpg" /&gt;&lt;/span&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;Thanks and Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.63636302948px;"&gt;Anil Ghadiya&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 09:36:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347620#M48131</guid>
      <dc:creator>anilghadiya</dc:creator>
      <dc:date>2014-12-17T09:36:24Z</dc:date>
    </item>
    <item>
      <title>Re: Error while before boot script on Saber Lite 6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347621#M48132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First off, please paste text into messages like this instead of using screen-shots. That allows e-mail notifications to contain the details in question and allows for quoting of the content.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Secondly, I'm sorry, but I can't spend cycles debugging your hardware. My suggestions about where to look were just that: suggestions of directions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MUX_CTL_PAD_x registers have an SION bit that allow you to see the state of pins through the corresponding GPIOX_PSR registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sure you'll find that the processor is seeing either or both the I2Cx_SDA or I2Cx_SCL pins low during the boot process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, note that the I2C accesses in question stem from the U-Boot code that tries to automatically identify the touch controllers commonly used on our boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's highly likely that these accesses aren't needed on your custom hardware. I presume that you know what display you're using and don't need auto-detect. This should be dealt with in your custom U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 15:32:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-before-boot-script-on-Saber-Lite-6Q/m-p/347621#M48132</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-12-17T15:32:10Z</dc:date>
    </item>
  </channel>
</rss>