<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 I.MX 6SoloX (Single step debug M4)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347296#M48071</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to Chapter 13 the ETM trace buffer and Trace port are accessible from the ARM Cortex A9, but how about single single step registers?&amp;nbsp; i.e I'm trying to some how debug the ARM M4 via the ARM 9.&amp;nbsp; So, no external debug SWD HW is required.&amp;nbsp; is it possible? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 01 Mar 2015 20:48:35 GMT</pubDate>
    <dc:creator>tcmichals</dc:creator>
    <dc:date>2015-03-01T20:48:35Z</dc:date>
    <item>
      <title>I.MX 6SoloX (Single step debug M4)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347296#M48071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to Chapter 13 the ETM trace buffer and Trace port are accessible from the ARM Cortex A9, but how about single single step registers?&amp;nbsp; i.e I'm trying to some how debug the ARM M4 via the ARM 9.&amp;nbsp; So, no external debug SWD HW is required.&amp;nbsp; is it possible? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Mar 2015 20:48:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347296#M48071</guid>
      <dc:creator>tcmichals</dc:creator>
      <dc:date>2015-03-01T20:48:35Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX 6SoloX (Single step debug M4)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347297#M48072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not an expert in the debug system but this statement in the RM makes me think it is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Internal access to on-chip buses and other interfaces are provided by the access ports&lt;/P&gt;&lt;P&gt;(APs). The available APs are:&lt;/P&gt;&lt;P&gt;• AHB-AP which provides an AHB-Lite master for access to a system AHB bus.&lt;/P&gt;&lt;P&gt;• APB-AP which provides an AMBA 3 APB master for access to the Debug APB that&lt;/P&gt;&lt;P&gt;configures all CoreSight components.&lt;/P&gt;&lt;P&gt;• JTAG-AP which provides JTAG access to on-chip components and operates as a&lt;/P&gt;&lt;P&gt;JTAG master port to drive JTAG chains throughout the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I know the ETM trace buffer is just iRAM used for trace and therefore it can be accessed by both cores.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me keep delving into this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2015 19:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347297#M48072</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-03-03T19:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX 6SoloX (Single step debug M4)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347298#M48073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alejandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for looking into this. I agree about the trace buffer. The goal is to create a simple gdb-server to access the HW debug registers directly, nmap the memory to user space. &lt;/P&gt;&lt;P&gt;(Wish I could get a sabre board to try this on :smileywink:)&lt;/P&gt;&lt;H3 class="r"&gt;&lt;/H3&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2015 19:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347298#M48073</guid>
      <dc:creator>tcmichals</dc:creator>
      <dc:date>2015-03-05T19:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX 6SoloX (Single step debug M4)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347299#M48074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Other solution, maybe not an elegant solution is the next.&lt;/P&gt;&lt;P&gt;I have seen a few MCUs used as JTAG programmers, that use an SPI port.&amp;nbsp; You could try to create your firmware and use the SPI module and hook connect the corresponding signals to the JTAG interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2015 20:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-6SoloX-Single-step-debug-M4/m-p/347299#M48074</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-03-05T20:13:15Z</dc:date>
    </item>
  </channel>
</rss>