<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: MX6 IPU_1task  block</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX6-IPU-1task-block/m-p/345890#M47755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiaoqiang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;24bit lcd support is described below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-93617"&gt;iMX6QD How to Add 24-bit LVDS Support in Android&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/434875"&gt;Re: 24bit LVDS display looks like wrong color depth on imx6DL AI PDK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also if this lvds lcd has different timings, than one used with Freescale Sabre board&lt;/P&gt;&lt;P&gt;(Hannstar lcd), one will have to change fb_videomode, example can be found below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://lists.denx.de/pipermail/u-boot/2012-May/125483.html" title="http://lists.denx.de/pipermail/u-boot/2012-May/125483.html"&gt;[U-Boot] [PATCH 9/9] mx6qsabrelite: Add splaschscreen support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 21 Dec 2014 14:07:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-12-21T14:07:37Z</dc:date>
    <item>
      <title>MX6 IPU_1task  block</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6-IPU-1task-block/m-p/345889#M47754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on our own designed board based i.MX6Q.Now I connected a 24-bit LVDS panels(4 pairs of LVDS data signals )&lt;/P&gt;&lt;P&gt;to LVDS0 port.And my bootargs for video is:   video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24.&lt;/P&gt;&lt;P&gt;When I boot up linux,my panel can only display some black and white vertical lines like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And some messages about IPU appeard:&lt;/P&gt;&lt;P&gt;Freeing init memory: 212K &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:378 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;ipu1_task D 80544b9c 0 378 2 0x00000000 &lt;/P&gt;&lt;P&gt;[&amp;lt;80544b9c&amp;gt;] (__schedule&lt;EM&gt;0x258/0x6d4) from [&amp;lt;803d2494&amp;gt;] (ipu_task_thread&lt;/EM&gt;0x260/0xaf0) &lt;/P&gt;&lt;P&gt;[&amp;lt;803d2494&amp;gt;] (ipu_task_thread&lt;EM&gt;0x260/0xaf0) from [&amp;lt;800943ec&amp;gt;] (kthread&lt;/EM&gt;0x80/0x88) &lt;/P&gt;&lt;P&gt;[&amp;lt;800943ec&amp;gt;] (kthread&lt;EM&gt;0x80/0x88) from [&amp;lt;80043a5c&amp;gt;] (kernel_thread_exit&lt;/EM&gt;0x0/0x8) &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:379 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;ipu1_task D 80544b9c 0 379 2 0x00000000 &lt;/P&gt;&lt;P&gt;[&amp;lt;80544b9c&amp;gt;] (__schedule&lt;EM&gt;0x258/0x6d4) from [&amp;lt;803d2494&amp;gt;] (ipu_task_thread&lt;/EM&gt;0x260/0xaf0) &lt;/P&gt;&lt;P&gt;[&amp;lt;803d2494&amp;gt;] (ipu_task_thread&lt;EM&gt;0x260/0xaf0) from [&amp;lt;800943ec&amp;gt;] (kthread&lt;/EM&gt;0x80/0x88) &lt;/P&gt;&lt;P&gt;[&amp;lt;800943ec&amp;gt;] (kthread&lt;EM&gt;0x80/0x88) from [&amp;lt;80043a5c&amp;gt;] (kernel_thread_exit&lt;/EM&gt;0x0/0x8) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Starting Advanced Power Management daemon... [80G [74G[ OK ] &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Last login: Thu Jan 1 00:01:37 UTC 1970 on ttymxc0 &lt;/P&gt;&lt;P&gt;speech-dispatcher disabled; edit /etc/default/speech-dispatcher &lt;/P&gt;&lt;P&gt;Checking for running unattended-upgrades: &lt;/P&gt;&lt;P&gt;vgaarb: this pci device is not a vga device &lt;/P&gt;&lt;P&gt;vgaarb: this pci device is not a vga device &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Starting bluetooth [80G [74G[ OK ] &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;[33m* [39;49m PulseAudio configured for per-user sessions &lt;/P&gt;&lt;P&gt;saned disabled; edit /etc/default/saned &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:378 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:379 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;1 Jan 00:00:47 ntpdate[5657]: no server suitable for synchronization found &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:378 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:379 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:378 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;INFO: task ipu1_task:379 blocked for more than 10 seconds. &lt;/P&gt;&lt;P&gt;"echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message. &lt;/P&gt;&lt;P&gt;I think maybe there is some relationship about my LVDS failure.But my HDMI is working OK.&lt;/P&gt;&lt;P&gt;Any advice will be appreciated.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Xiaoqiang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Dec 2014 03:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6-IPU-1task-block/m-p/345889#M47754</guid>
      <dc:creator>xiaoqiangyang</dc:creator>
      <dc:date>2014-12-12T03:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: MX6 IPU_1task  block</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6-IPU-1task-block/m-p/345890#M47755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiaoqiang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;24bit lcd support is described below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-93617"&gt;iMX6QD How to Add 24-bit LVDS Support in Android&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/434875"&gt;Re: 24bit LVDS display looks like wrong color depth on imx6DL AI PDK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also if this lvds lcd has different timings, than one used with Freescale Sabre board&lt;/P&gt;&lt;P&gt;(Hannstar lcd), one will have to change fb_videomode, example can be found below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://lists.denx.de/pipermail/u-boot/2012-May/125483.html" title="http://lists.denx.de/pipermail/u-boot/2012-May/125483.html"&gt;[U-Boot] [PATCH 9/9] mx6qsabrelite: Add splaschscreen support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Dec 2014 14:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6-IPU-1task-block/m-p/345890#M47755</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-21T14:07:37Z</dc:date>
    </item>
  </channel>
</rss>