<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックrunning clutter based application on imx53</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/running-clutter-based-application-on-imx53/m-p/345688#M47717</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am trying to execute a clutter based application on the imx53qsb board but am getting errors. &lt;BR /&gt;i used the fsl-bsp dora to butbake core-image-sato and IMAGE_INSTALLed packagegroup-core-clutter-core&lt;/P&gt;&lt;P&gt;clutter code compiles without error but on execution i get the error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GModule-CRITICAL **: g_module_close: 'module-&amp;gt;ref_count &amp;gt; 0' failed&lt;/P&gt;&lt;P&gt;Clutter-CRITICAL **: Unable to initialize Clutter: Failed to connected to any renderer due to constraints&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am not sure where the problem is coming from or what to configure for it.&lt;/P&gt;&lt;P&gt;simple_draw 1000, es11ex works fine for opengl testing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anybody got any clutter app on imx53 working .. your method used is welcomed..&lt;/P&gt;&lt;P&gt;anybody with any idea is welcomed to help and ask any specific question if need...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:RAYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Aug 2014 10:17:41 GMT</pubDate>
    <dc:creator>rayssadet</dc:creator>
    <dc:date>2014-08-08T10:17:41Z</dc:date>
    <item>
      <title>running clutter based application on imx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/running-clutter-based-application-on-imx53/m-p/345688#M47717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am trying to execute a clutter based application on the imx53qsb board but am getting errors. &lt;BR /&gt;i used the fsl-bsp dora to butbake core-image-sato and IMAGE_INSTALLed packagegroup-core-clutter-core&lt;/P&gt;&lt;P&gt;clutter code compiles without error but on execution i get the error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GModule-CRITICAL **: g_module_close: 'module-&amp;gt;ref_count &amp;gt; 0' failed&lt;/P&gt;&lt;P&gt;Clutter-CRITICAL **: Unable to initialize Clutter: Failed to connected to any renderer due to constraints&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am not sure where the problem is coming from or what to configure for it.&lt;/P&gt;&lt;P&gt;simple_draw 1000, es11ex works fine for opengl testing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anybody got any clutter app on imx53 working .. your method used is welcomed..&lt;/P&gt;&lt;P&gt;anybody with any idea is welcomed to help and ask any specific question if need...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:RAYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Aug 2014 10:17:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/running-clutter-based-application-on-imx53/m-p/345688#M47717</guid>
      <dc:creator>rayssadet</dc:creator>
      <dc:date>2014-08-08T10:17:41Z</dc:date>
    </item>
    <item>
      <title>Re: running clutter based application on imx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/running-clutter-based-application-on-imx53/m-p/345689#M47718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I investigated and unfortunately it seems that clutter is not working on i.MX53 but there is an append (link below)to get it running on the i.MX6, in case it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/tree/recipes-graphics/clutter/clutter-1.0_%25.bbappend"&gt;http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/tree/recipes-graphics/clutter/clutter-1.0_%25.bbappend&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Sep 2014 20:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/running-clutter-based-application-on-imx53/m-p/345689#M47718</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2014-09-11T20:09:07Z</dc:date>
    </item>
  </channel>
</rss>