<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPerformance boost by writing an application in Kernel space rather than kernel space</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Performance-boost-by-writing-an-application-in-Kernel-space/m-p/345686#M47715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to write an application, which will better choice !! &lt;/P&gt;&lt;P&gt;&amp;nbsp; 1. Writing a simple application in the User space and invoked during startup and run the system forever. (It seems to be easy but not meeting the time critical event) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(or)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Configure the kernel and disable the unwanted hardware modules and put the application in to the kernel thread. So it will be preemptive and tightly packed with less latency.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Feb 2015 23:09:51 GMT</pubDate>
    <dc:creator>lyfsci</dc:creator>
    <dc:date>2015-02-27T23:09:51Z</dc:date>
    <item>
      <title>Performance boost by writing an application in Kernel space rather than kernel space</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-boost-by-writing-an-application-in-Kernel-space/m-p/345686#M47715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to write an application, which will better choice !! &lt;/P&gt;&lt;P&gt;&amp;nbsp; 1. Writing a simple application in the User space and invoked during startup and run the system forever. (It seems to be easy but not meeting the time critical event) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(or)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Configure the kernel and disable the unwanted hardware modules and put the application in to the kernel thread. So it will be preemptive and tightly packed with less latency.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2015 23:09:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-boost-by-writing-an-application-in-Kernel-space/m-p/345686#M47715</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2015-02-27T23:09:51Z</dc:date>
    </item>
    <item>
      <title>Re: Performance boost by writing an application in Kernel space rather than kernel space</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-boost-by-writing-an-application-in-Kernel-space/m-p/345687#M47716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lyf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general performance is similar in both cases, however advantage&lt;/P&gt;&lt;P&gt;of user space application is that OS do not allow it to do bad things like&lt;/P&gt;&lt;P&gt;crashing the machine. You can refer below links for details since this is&lt;/P&gt;&lt;P&gt;generic linux question&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.tldp.org/FAQ/Threads-FAQ/Types.html" title="http://www.tldp.org/FAQ/Threads-FAQ/Types.html"&gt;Linux Threads Home Page: What are threads (user/kernel)?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://stackoverflow.com/questions/5957570/what-is-the-difference-between-the-kernel-space-and-the-user-space" title="http://stackoverflow.com/questions/5957570/what-is-the-difference-between-the-kernel-space-and-the-user-space"&gt;operating system - What is the difference between the kernel space and the user space? - Stack Overflow&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2015 01:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-boost-by-writing-an-application-in-Kernel-space/m-p/345687#M47716</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-03T01:01:17Z</dc:date>
    </item>
  </channel>
</rss>