<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TFTP boot process does not connect in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TFTP-boot-process-does-not-connect/m-p/344894#M47585</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been using the latest u-boot from our latest BSP using Yocto with the imx6Q and it is working. My tftp server is in a Linux Machine.&lt;/P&gt;&lt;P&gt;Which board are you using? Have you tried with a different client (different to your PC)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Nov 2014 16:06:42 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2014-11-24T16:06:42Z</dc:date>
    <item>
      <title>TFTP boot process does not connect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTP-boot-process-does-not-connect/m-p/344893#M47584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to load an image via tftp using the complete command&lt;/P&gt;&lt;P&gt;$:&amp;gt; tftpboot 12000000 172.30.50.125:uImage&lt;/P&gt;&lt;P&gt;to download an uImage from ip address 172.30.50.125.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My tftp server is a Tftpd32 running on Win XP, but - I cannot see a connection coming in in the corresponding logging window, no peer, no requested file gets mentioned. It just runs into timeout(s)&lt;/P&gt;&lt;P&gt;My Hyperterminal log is:&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;STRONG&gt;U-Boot &amp;gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;STRONG&gt;U-Boot &amp;gt; tftpboot 12000000 172.30.50.125:uImage&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Using FEC device&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;TFTP from server 172.30.50.125; our IP address is 172.30.50.175&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Filename 'uImage'.&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Load address: 0x12000000&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Loading: T T T T T T T T T T&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Retry count exceeded; starting again&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Using FEC device&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;TFTP from server 172.30.50.125; our IP address is 172.30.50.175&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Filename 'uImage'.&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Load address: 0x12000000&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Loading: T ................&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;STRONG&gt;Abort&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;STRONG&gt;U-Boot &amp;gt; ping 172.30.50.125&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Using FEC device&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;host 172.30.50.125 is alive&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;STRONG&gt;U-Boot &amp;gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I aborted using Ctrl-C, otherwise it would go on trying to download/timeout.&lt;/P&gt;&lt;P&gt;What goes wrong, why can't I see any log in my Tftpd32 log window? If I use tftpd32 to download a file from the same host I can see a request log&lt;/P&gt;&lt;P&gt;That is the only tftp server I have to test it. Booting from SD card fails, stops at 'Starting kernel ...'. See my other question..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If someone knows help...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Juergen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Nov 2014 12:30:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTP-boot-process-does-not-connect/m-p/344893#M47584</guid>
      <dc:creator>juergenvorbach</dc:creator>
      <dc:date>2014-11-17T12:30:09Z</dc:date>
    </item>
    <item>
      <title>Re: TFTP boot process does not connect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTP-boot-process-does-not-connect/m-p/344894#M47585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been using the latest u-boot from our latest BSP using Yocto with the imx6Q and it is working. My tftp server is in a Linux Machine.&lt;/P&gt;&lt;P&gt;Which board are you using? Have you tried with a different client (different to your PC)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2014 16:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTP-boot-process-does-not-connect/m-p/344894#M47585</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-11-24T16:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: TFTP boot process does not connect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTP-boot-process-does-not-connect/m-p/344895#M47586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alejandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also have Ubuntu running in a virtual machine an I can successfully &lt;/P&gt;&lt;P&gt;connect to the tftp server running on this machine, but when I try to &lt;/P&gt;&lt;P&gt;connect to the tftpd32 process running on my XP laptop it doesn't &lt;/P&gt;&lt;P&gt;connect - can't see any logging messages. Thus it is connecting with &lt;/P&gt;&lt;P&gt;Ubuntu, I am happy with that for the moment, but I have to start the &lt;/P&gt;&lt;P&gt;virtual machine each time for this process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tftpd32 offers a tftp client itself on a different tab. If I use this &lt;/P&gt;&lt;P&gt;client to connect and download from the tftpd32 server it connects and &lt;/P&gt;&lt;P&gt;loads, so I think this server should be running and working - but it &lt;/P&gt;&lt;P&gt;doesn't connect from SABRE board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe there's a firewall blocking from external device - I don't know at &lt;/P&gt;&lt;P&gt;the moment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can live with the Ubuntu solution, but if someone knows how to solve &lt;/P&gt;&lt;P&gt;the tftpd32 issue, I would like to know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the SABRE 4core board, but haven't tested with other clients, &lt;/P&gt;&lt;P&gt;only from u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;     Juergen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Nov 2014 08:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTP-boot-process-does-not-connect/m-p/344895#M47586</guid>
      <dc:creator>juergenvorbach</dc:creator>
      <dc:date>2014-11-25T08:20:52Z</dc:date>
    </item>
  </channel>
</rss>