<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX Keypad no device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Keypad-no-device/m-p/344559#M47510</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have activated the keypad driver in the kernel and configured the column and row keypads in the board file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, in the device filesystem is no entry /dev/input/input0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have started debugging and see that the function "imx_keypad_init" is called to register the function pointer for probing and remove, but the function "imx_keypad_probe" is never called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has somebody an idea what could be the reason?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Sep 2014 05:55:36 GMT</pubDate>
    <dc:creator>Mark78</dc:creator>
    <dc:date>2014-09-25T05:55:36Z</dc:date>
    <item>
      <title>i.MX Keypad no device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Keypad-no-device/m-p/344559#M47510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have activated the keypad driver in the kernel and configured the column and row keypads in the board file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, in the device filesystem is no entry /dev/input/input0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have started debugging and see that the function "imx_keypad_init" is called to register the function pointer for probing and remove, but the function "imx_keypad_probe" is never called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has somebody an idea what could be the reason?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 05:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-Keypad-no-device/m-p/344559#M47510</guid>
      <dc:creator>Mark78</dc:creator>
      <dc:date>2014-09-25T05:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX Keypad no device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Keypad-no-device/m-p/344560#M47511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What board are you using and which BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Sep 2014 20:35:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-Keypad-no-device/m-p/344560#M47511</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-09-30T20:35:57Z</dc:date>
    </item>
  </channel>
</rss>