<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Windows embedded compact 2013 GPU source code in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Windows-embedded-compact-2013-GPU-source-code/m-p/344491#M47500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am facing issue with IMX6 solo with 512 MB RAM, when I run GPU sample application with 512 MB ram it crashes after ~5-10secs. But the same crash doesn't&amp;nbsp; happen for 1GB RAM. I suspect the memory range used for GPU is hard coded in the driver may cause the crash issue. To debug this i need source code for GPU driver(IMX6) Windows Embedded Compact 2013.&lt;/P&gt;&lt;P&gt;Can I get the source code for GPU driver (IMX6) Windows Embedded compact 2013?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Nov 2014 07:38:43 GMT</pubDate>
    <dc:creator>Jeslin</dc:creator>
    <dc:date>2014-11-17T07:38:43Z</dc:date>
    <item>
      <title>Windows embedded compact 2013 GPU source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-embedded-compact-2013-GPU-source-code/m-p/344491#M47500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am facing issue with IMX6 solo with 512 MB RAM, when I run GPU sample application with 512 MB ram it crashes after ~5-10secs. But the same crash doesn't&amp;nbsp; happen for 1GB RAM. I suspect the memory range used for GPU is hard coded in the driver may cause the crash issue. To debug this i need source code for GPU driver(IMX6) Windows Embedded Compact 2013.&lt;/P&gt;&lt;P&gt;Can I get the source code for GPU driver (IMX6) Windows Embedded compact 2013?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Nov 2014 07:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-embedded-compact-2013-GPU-source-code/m-p/344491#M47500</guid>
      <dc:creator>Jeslin</dc:creator>
      <dc:date>2014-11-17T07:38:43Z</dc:date>
    </item>
    <item>
      <title>Re: Windows embedded compact 2013 GPU source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-embedded-compact-2013-GPU-source-code/m-p/344492#M47501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/AdeneoEmbedded"&gt;AdeneoEmbedded&lt;/A&gt; , do you have information or can you help with this question?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Nov 2014 18:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-embedded-compact-2013-GPU-source-code/m-p/344492#M47501</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-11-17T18:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: Windows embedded compact 2013 GPU source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-embedded-compact-2013-GPU-source-code/m-p/344493#M47502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="jiveTT-hover-user jive-link-profile-small" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="204032" data-objecttype="3" href="https://community.nxp.com/people/AdeneoEmbedded"&gt;Adeneo Embedded&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Can you help me on this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 07:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-embedded-compact-2013-GPU-source-code/m-p/344493#M47502</guid>
      <dc:creator>Jeslin</dc:creator>
      <dc:date>2014-12-02T07:27:19Z</dc:date>
    </item>
  </channel>
</rss>