<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ECSPI Read and Write Timings in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-Read-and-Write-Timings/m-p/344305#M47453</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The hardware specs of i.MX6 Datasheet(s) regarding eCSPI timings are results&lt;/P&gt;&lt;P&gt;of tests. Requirements for reliable read are more strict than for writing. One of SPI &lt;BR /&gt;ideas is simultaneous read and write ops (implemented as a common shift register),&lt;/P&gt;&lt;P&gt;but there are devices that support SPI interface, but do not need both read and write&lt;BR /&gt;ops.&amp;nbsp; To say roughly we can use "slow" ADC and "fast" DAC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Oct 2014 02:43:25 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-10-23T02:43:25Z</dc:date>
    <item>
      <title>ECSPI Read and Write Timings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-Read-and-Write-Timings/m-p/344304#M47452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;On this document, en page 77:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf?fasp=1" title="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf?fasp=1"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf?fasp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The tclk timings are 43ns for Read and 15ns for Write.&lt;/P&gt;&lt;P&gt;However the ECSPI is a shift registry. So for each clk, there is a read and a write.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So what is the difference between "ECSPIx_SCLK Cycle Time–Read" and "ECSPIx_SCLK Cycle Time–Write" ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Philippe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 14:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-Read-and-Write-Timings/m-p/344304#M47452</guid>
      <dc:creator>philippechapet</dc:creator>
      <dc:date>2014-10-22T14:53:37Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI Read and Write Timings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-Read-and-Write-Timings/m-p/344305#M47453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The hardware specs of i.MX6 Datasheet(s) regarding eCSPI timings are results&lt;/P&gt;&lt;P&gt;of tests. Requirements for reliable read are more strict than for writing. One of SPI &lt;BR /&gt;ideas is simultaneous read and write ops (implemented as a common shift register),&lt;/P&gt;&lt;P&gt;but there are devices that support SPI interface, but do not need both read and write&lt;BR /&gt;ops.&amp;nbsp; To say roughly we can use "slow" ADC and "fast" DAC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Oct 2014 02:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-Read-and-Write-Timings/m-p/344305#M47453</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-10-23T02:43:25Z</dc:date>
    </item>
  </channel>
</rss>