<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6DQ operating temperature. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344087#M47394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For thermal design it is highly recommended to be oriented on &lt;BR /&gt;Tj max in the Datasheet (105 degree). &lt;BR /&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;To say simply - 106 degree must not be achievable.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Sep 2014 09:33:59 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-09-26T09:33:59Z</dc:date>
    <item>
      <title>i.MX6DQ operating temperature.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344082#M47389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our partner have a question about i.MX6DQ temperature.&lt;/P&gt;&lt;P&gt;Please see Table 6 in IMX6DQCEC Rev.3.&lt;/P&gt;&lt;P&gt;We can see Tj(max) = 105 degrees for extended consumer and 95 degrees for standard consumer products.&lt;/P&gt;&lt;P&gt;According to AN4724, I guess no damage for i.MX6DQ if i.MX6DQ works Tj = 105 degrees (or 95 degrees) all of the time, and &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;it has some margin to the temperature (Tj) that break down i.MX6DQ.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is correct, could you let me know the temperature (Tj) that bread down i.MX6DQ?&lt;/P&gt;&lt;P&gt;I guess i.MX6DQ is broken when Tj = 150 degrees because TSTORAGE(max) = 150 degrees in Table 4.&lt;/P&gt;&lt;P&gt;Is this right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 02:17:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344082#M47389</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-09-25T02:17:48Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DQ operating temperature.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344083#M47390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; You are right, IMX6DQ will work correctly (and meet&amp;nbsp; all hardware specs in i.MX6 DQ Datasheet)&lt;/P&gt;&lt;P&gt;while Tj &amp;lt;= 105 (or 95) degree C. And, strictly speaking, we cannot guarantee proper operations&lt;/P&gt;&lt;P&gt;for Tj &amp;gt; 105 degree C. Maximal temperature of 150 degree C relates to storage environment,&lt;/P&gt;&lt;P&gt;assuming the device is not under working conditions. It is clear if environment temperature is&lt;/P&gt;&lt;P&gt;greater than 150 degree C IMX6DQ may be broken.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 03:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344083#M47390</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-09-25T03:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DQ operating temperature.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344084#M47391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;To make sure, I have one more question.&lt;/P&gt;&lt;P&gt;If use under 105 degree C &amp;lt; Tj &amp;lt; 150 degree C, Freescale cannot guarantee proper operations, but I guess i.MX6DQ is not broken.&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 08:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344084#M47391</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-09-25T08:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DQ operating temperature.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344085#M47392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Strictly speaking 150 degree C is specified for storage enviromment ; at least, &lt;BR /&gt;i.MX6 is not powered. Your approach may be used just for rough estimations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 08:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344085#M47392</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-09-25T08:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DQ operating temperature.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344086#M47393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Strictly speaking 150 degree C is specified for storage enviromment&lt;/P&gt;&lt;P&gt;Yes, I understandd.&lt;/P&gt;&lt;P&gt;Actually, we want to know how much margin should we estimate when thermal design.&lt;/P&gt;&lt;P&gt;If i.MX6DQ is damaged when over 105 degree C even little, we have to prepare some margin when thermal design to prevent over 105 degree C.&lt;/P&gt;&lt;P&gt;(e.g. 105 * 0.8 = 84 degree C)&lt;/P&gt;&lt;P&gt;So we want to know the temperature i.MX6DQ is damaged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 09:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344086#M47393</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-09-25T09:27:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DQ operating temperature.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344087#M47394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For thermal design it is highly recommended to be oriented on &lt;BR /&gt;Tj max in the Datasheet (105 degree). &lt;BR /&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;To say simply - 106 degree must not be achievable.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 09:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-operating-temperature/m-p/344087#M47394</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-09-26T09:33:59Z</dc:date>
    </item>
  </channel>
</rss>