<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUSB Multitouch Panel on i.MX6 (Sabre Lite) board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Multitouch-Panel-on-i-MX6-Sabre-Lite-board/m-p/343544#M47321</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone been able to get a USB multitouch screen or screen overlay working on an i.MX6? I'm using the Sabre Lite board (BD-SL-i.MX6) from Boundary Devices, running a Yocto Daisy build with the 3.10.17 kernel. The screen I have happens to be a "USBest Technology SiS HID Touch Controller." It implements the HID-multitouch standard, and it shows up and works fine on a standard x86 PC with a recent version of Ubuntu (so I know the screen fundamentally works with Linux and the HID-multitouch driver).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I build the kernel and enable the HID-Multitouch kernel module, plugging in the panel just gives me a repeated output over and over in dmesg like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;usb 1-1.2: new full-speed USB device number 58 using ci_hdrc&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: not running at top speed; connect to a high speed hub&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; input: USBest Technology SiS HID Touch Controller as /devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.2/1-1.2:1.0/input/input553&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; hid-multitouch 0003:0457:0817.0229: input: USB HID v1.00 Mouse [USBest Technology SiS HID Touch Controller] on usb-ci_hdrc.1-1.2/input0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: USB disconnect, device number 58&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: new full-speed USB device number 59 using ci_hdrc&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: not running at top speed; connect to a high speed hub&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; input: USBest Technology SiS HID Touch Controller as /devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.2/1-1.2:1.0/input/input554&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; hid-multitouch 0003:0457:0817.022A: input: USB HID v1.00 Mouse [USBest Technology SiS HID Touch Controller] on usb-ci_hdrc.1-1.2/input0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: USB disconnect, device number 59&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically, it looks like the device is being found by the HID-multitouch driver, but for some reason it keeps disconnecting it immediately after, then trying again, over and over again. Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Aug 2014 20:30:53 GMT</pubDate>
    <dc:creator>sgerenser</dc:creator>
    <dc:date>2014-08-07T20:30:53Z</dc:date>
    <item>
      <title>USB Multitouch Panel on i.MX6 (Sabre Lite) board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Multitouch-Panel-on-i-MX6-Sabre-Lite-board/m-p/343544#M47321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone been able to get a USB multitouch screen or screen overlay working on an i.MX6? I'm using the Sabre Lite board (BD-SL-i.MX6) from Boundary Devices, running a Yocto Daisy build with the 3.10.17 kernel. The screen I have happens to be a "USBest Technology SiS HID Touch Controller." It implements the HID-multitouch standard, and it shows up and works fine on a standard x86 PC with a recent version of Ubuntu (so I know the screen fundamentally works with Linux and the HID-multitouch driver).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I build the kernel and enable the HID-Multitouch kernel module, plugging in the panel just gives me a repeated output over and over in dmesg like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;usb 1-1.2: new full-speed USB device number 58 using ci_hdrc&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: not running at top speed; connect to a high speed hub&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; input: USBest Technology SiS HID Touch Controller as /devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.2/1-1.2:1.0/input/input553&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; hid-multitouch 0003:0457:0817.0229: input: USB HID v1.00 Mouse [USBest Technology SiS HID Touch Controller] on usb-ci_hdrc.1-1.2/input0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: USB disconnect, device number 58&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: new full-speed USB device number 59 using ci_hdrc&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: not running at top speed; connect to a high speed hub&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; input: USBest Technology SiS HID Touch Controller as /devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.2/1-1.2:1.0/input/input554&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; hid-multitouch 0003:0457:0817.022A: input: USB HID v1.00 Mouse [USBest Technology SiS HID Touch Controller] on usb-ci_hdrc.1-1.2/input0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt; usb 1-1.2: USB disconnect, device number 59&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically, it looks like the device is being found by the HID-multitouch driver, but for some reason it keeps disconnecting it immediately after, then trying again, over and over again. Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Aug 2014 20:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Multitouch-Panel-on-i-MX6-Sabre-Lite-board/m-p/343544#M47321</guid>
      <dc:creator>sgerenser</dc:creator>
      <dc:date>2014-08-07T20:30:53Z</dc:date>
    </item>
  </channel>
</rss>