<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mipi</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mipi/m-p/343516#M47317</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sumo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for hdmi input one can use parallel input (csi), for input through mipi one will have&lt;/P&gt;&lt;P&gt;to use additional external converter and modify sources, as below :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/328301"&gt;Some Experience When Enable MIPI Camera&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="314211" data-objecttype="1" href="https://community.freescale.com/thread/314211"&gt;https://community.freescale.com/thread/314211&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Jan 2015 00:20:44 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-15T00:20:44Z</dc:date>
    <item>
      <title>mipi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mipi/m-p/343515#M47316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi imx community&lt;/P&gt;&lt;P&gt;i have ov5640 mipi of econsystem and i found that the driver (ov5640_mipi of 3.10.17 kernel) doesnt contain any registers configuration for hdmi.&lt;/P&gt;&lt;P&gt;did anyone managed to use hdmi anyhow with the driver mentioned above?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 12:41:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mipi/m-p/343515#M47316</guid>
      <dc:creator>sumosumo</dc:creator>
      <dc:date>2015-01-14T12:41:38Z</dc:date>
    </item>
    <item>
      <title>Re: mipi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mipi/m-p/343516#M47317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sumo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for hdmi input one can use parallel input (csi), for input through mipi one will have&lt;/P&gt;&lt;P&gt;to use additional external converter and modify sources, as below :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/328301"&gt;Some Experience When Enable MIPI Camera&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="314211" data-objecttype="1" href="https://community.freescale.com/thread/314211"&gt;https://community.freescale.com/thread/314211&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jan 2015 00:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mipi/m-p/343516#M47317</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-15T00:20:44Z</dc:date>
    </item>
  </channel>
</rss>