<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx53 wakeup source</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx53-wakeup-source/m-p/343417#M47281</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, thanks.&lt;/P&gt;&lt;P&gt;I've checked it - saving the contents of PND0..4 just after exiting suspend state does it. The register has the bit set of the interrupt, that led to resume.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Jan 2015 16:10:05 GMT</pubDate>
    <dc:creator>alexandervarnin</dc:creator>
    <dc:date>2015-01-17T16:10:05Z</dc:date>
    <item>
      <title>imx53 wakeup source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-wakeup-source/m-p/343415#M47279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my configuration I use imx53 CPU with Linux kernel 2.6.35 (from freescale). It has two wake up sources from the low-power state - RTC and gpio pin (as interrupt).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to determine after the wakeup, what was the source (the reason) of the wakeup event?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked through imx53 reference manual, but failed to find this information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 12:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-wakeup-source/m-p/343415#M47279</guid>
      <dc:creator>alexandervarnin</dc:creator>
      <dc:date>2015-01-14T12:13:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx53 wakeup source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-wakeup-source/m-p/343416#M47280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexander,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been delving into that and I wonder if you have checked the TZIC module?&lt;/P&gt;&lt;P&gt;My suggestion is to check the TZIC_PNDn register and see if the corresponding flags are set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jan 2015 20:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-wakeup-source/m-p/343416#M47280</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-01-15T20:22:07Z</dc:date>
    </item>
    <item>
      <title>Re: imx53 wakeup source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-wakeup-source/m-p/343417#M47281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, thanks.&lt;/P&gt;&lt;P&gt;I've checked it - saving the contents of PND0..4 just after exiting suspend state does it. The register has the bit set of the interrupt, that led to resume.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Jan 2015 16:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-wakeup-source/m-p/343417#M47281</guid>
      <dc:creator>alexandervarnin</dc:creator>
      <dc:date>2015-01-17T16:10:05Z</dc:date>
    </item>
  </channel>
</rss>