<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6 camera preview IPU functionality in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-camera-preview-IPU-functionality/m-p/343148#M47219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;there is a "camera preview" function in iMX's image processing unit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;User guide explanation is very short:&lt;/P&gt;&lt;P&gt;37.1.2.1.6.3 Camera Preview&lt;/P&gt;&lt;P&gt;• Tearing artifacts can be prevented by (automatic) page-flip double buffering in&lt;/P&gt;&lt;P&gt;system memory&lt;/P&gt;&lt;P&gt;• Alternatively, the&lt;STRONG&gt; video stream from an image sensor can be sent directly to the&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;display&lt;/STRONG&gt; buffer used for screen refresh. The significance of this option is that only a&lt;/P&gt;&lt;P&gt;single frame buffer is needed (and not two). This buffer may be located either in&lt;/P&gt;&lt;P&gt;system memory or in an external display controller.&lt;/P&gt;&lt;P&gt;• This option is useful, e.g., in a low frame rate, when tearing is not visible.&lt;/P&gt;&lt;P&gt;• When tearing must be prevented, the refresh cycle in the display can be&lt;/P&gt;&lt;P&gt;synchronized with the timing signals from the sensor (two refresh cycles for each&lt;/P&gt;&lt;P&gt;input frame): the IPU receives a VSYNC signal from the sensor and generates&lt;/P&gt;&lt;P&gt;from it synchronization signals for the display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is: how to configure IPU to stream video directly from sensor to screen without CPU interaction?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Main idea to implement "instant start" appearence, show video from bootloader and then start linux.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Dec 2014 09:24:45 GMT</pubDate>
    <dc:creator>uSasha</dc:creator>
    <dc:date>2014-12-11T09:24:45Z</dc:date>
    <item>
      <title>iMX6 camera preview IPU functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-camera-preview-IPU-functionality/m-p/343148#M47219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;there is a "camera preview" function in iMX's image processing unit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;User guide explanation is very short:&lt;/P&gt;&lt;P&gt;37.1.2.1.6.3 Camera Preview&lt;/P&gt;&lt;P&gt;• Tearing artifacts can be prevented by (automatic) page-flip double buffering in&lt;/P&gt;&lt;P&gt;system memory&lt;/P&gt;&lt;P&gt;• Alternatively, the&lt;STRONG&gt; video stream from an image sensor can be sent directly to the&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;display&lt;/STRONG&gt; buffer used for screen refresh. The significance of this option is that only a&lt;/P&gt;&lt;P&gt;single frame buffer is needed (and not two). This buffer may be located either in&lt;/P&gt;&lt;P&gt;system memory or in an external display controller.&lt;/P&gt;&lt;P&gt;• This option is useful, e.g., in a low frame rate, when tearing is not visible.&lt;/P&gt;&lt;P&gt;• When tearing must be prevented, the refresh cycle in the display can be&lt;/P&gt;&lt;P&gt;synchronized with the timing signals from the sensor (two refresh cycles for each&lt;/P&gt;&lt;P&gt;input frame): the IPU receives a VSYNC signal from the sensor and generates&lt;/P&gt;&lt;P&gt;from it synchronization signals for the display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is: how to configure IPU to stream video directly from sensor to screen without CPU interaction?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Main idea to implement "instant start" appearence, show video from bootloader and then start linux.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Dec 2014 09:24:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-camera-preview-IPU-functionality/m-p/343148#M47219</guid>
      <dc:creator>uSasha</dc:creator>
      <dc:date>2014-12-11T09:24:45Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 camera preview IPU functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-camera-preview-IPU-functionality/m-p/343149#M47220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at SDK example and sect.18.5 CSI preview&lt;/P&gt;&lt;P&gt;iMX6_Firmware_Guide.pdf (included to SDK) &lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Bare-metal SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Dec 2014 10:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-camera-preview-IPU-functionality/m-p/343149#M47220</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-11T10:52:26Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 camera preview IPU functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-camera-preview-IPU-functionality/m-p/343150#M47221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Igor!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Dec 2014 13:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-camera-preview-IPU-functionality/m-p/343150#M47221</guid>
      <dc:creator>uSasha</dc:creator>
      <dc:date>2014-12-11T13:58:45Z</dc:date>
    </item>
  </channel>
</rss>