<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx28 and RESETN problem. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx28-and-RESETN-problem/m-p/342880#M47147</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi fear&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;recommended way to do RESETN is to remove VDD5V&lt;/P&gt;&lt;P&gt;(as i.mx28 EVK is doind&amp;nbsp; with MOSFET), that is as at&lt;/P&gt;&lt;P&gt;power-up. Otherwise one can encounter with weird problems,&lt;/P&gt;&lt;P&gt;for example VDD4P2 is disabled at reset according to sect.&lt;/P&gt;&lt;P&gt;11.12.9 DC-DC Converter 4.2V Control Register&lt;/P&gt;&lt;P&gt;(HW_POWER_DCDC4P2) , bit ENABLE_4P2 =0 &lt;A href="http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;MCIMX28RM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Sep 2014 23:46:19 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-09-05T23:46:19Z</dc:date>
    <item>
      <title>i.mx28 and RESETN problem.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx28-and-RESETN-problem/m-p/342879#M47146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hi all,&lt;/P&gt;&lt;P&gt; I have problem with RESETN and i.mx28. I use VDD5V power supply only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; i use external watchdog IC for generate RESETN signal. For test i am not refresh wdg and after some good reboots(10-50) my i.mx28 go to hang state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;vddxtal - 0.97&lt;/P&gt;&lt;P&gt;dcdc_vddio_3v3 - 3.0&lt;/P&gt;&lt;P&gt;vdd4p2 - 0.3V&lt;/P&gt;&lt;P&gt;dcdc_vddd_1v2 - 1.0V&lt;/P&gt;&lt;P&gt;dcdc_vdda_1v8 - 0.96&lt;/P&gt;&lt;P&gt;vdd5v 4.95v&lt;/P&gt;&lt;P&gt;Clock on 24Mhz - are present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and only one way to out from this hang state - remove power and apply it again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use boot from NAND flash and then "hang" happend i cant see any chip selects signal GPMI_CS0.&lt;/P&gt;&lt;P&gt;and in debug serial not any debug info.&lt;/P&gt;&lt;P&gt;Is this possible that internal bootloader are "hang"? Where i can see bootloader code for understand why boot stopped.&lt;/P&gt;&lt;P&gt;Is this possible that internal LDO (VDD5V to VDD4P2) go to current limit state? But why reasserting RESETN not restore it.&lt;/P&gt;&lt;P&gt;On my board i supply only DDR, NAND and i.mx from internal i.mx power sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why on i.mx28 EVK added MOSFET for break VDD5V then reset button pressed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Sep 2014 12:23:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx28-and-RESETN-problem/m-p/342879#M47146</guid>
      <dc:creator>fear_nada</dc:creator>
      <dc:date>2014-09-05T12:23:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx28 and RESETN problem.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx28-and-RESETN-problem/m-p/342880#M47147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi fear&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;recommended way to do RESETN is to remove VDD5V&lt;/P&gt;&lt;P&gt;(as i.mx28 EVK is doind&amp;nbsp; with MOSFET), that is as at&lt;/P&gt;&lt;P&gt;power-up. Otherwise one can encounter with weird problems,&lt;/P&gt;&lt;P&gt;for example VDD4P2 is disabled at reset according to sect.&lt;/P&gt;&lt;P&gt;11.12.9 DC-DC Converter 4.2V Control Register&lt;/P&gt;&lt;P&gt;(HW_POWER_DCDC4P2) , bit ENABLE_4P2 =0 &lt;A href="http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;MCIMX28RM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Sep 2014 23:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx28-and-RESETN-problem/m-p/342880#M47147</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-05T23:46:19Z</dc:date>
    </item>
  </channel>
</rss>