<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB Serial Downloader mode - IMX6 Quad in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342651#M47115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am seeing this behavior on two boards that we have built. I am not suspecting any inadvertent shorts as SBRM2 values changes as per the setting done by the switches. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Sep 2014 11:24:38 GMT</pubDate>
    <dc:creator>rajniks</dc:creator>
    <dc:date>2014-09-10T11:24:38Z</dc:date>
    <item>
      <title>USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342645#M47109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom board design in which USB Serial down-loader mode doesn't seem to work. I have been able to connect Lauterbach debugger directly but have not been successful with serial downloader mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my board, I have connected USB_OTG_ID to pin T4 which has ALT3 functionality as OTG_ID. Will this create a problem as I can see on Sabre Smart OTG_ID is connected to Pin W23 which has ALT0 functionality as OTG_ID. Please let me know if the Freescale internal boot code looks only at one of these in order to decide to boot as USB device or host mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Sep 2014 09:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342645#M47109</guid>
      <dc:creator>rajniks</dc:creator>
      <dc:date>2014-09-05T09:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342646#M47110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;iROM code does not check OTG_ID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Sep 2014 09:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342646#M47110</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-05T09:55:28Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342647#M47111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem on my custom board looks like the processor is not going into correct boot mode by switch setting. I initially had a 10K pull down and switch to connect 3.3V. While experimenting when I pull down both the lines to low which is actually "boot from fuses mode" my board gets detected as USB Device and I am able to connect DDR Tester software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to configure the serial downloader mode by setting boot mode pin 0 as 3.3V and&amp;nbsp; pin 1 as pull down nothing happens. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why would such a problem exists. I have checked the state of both the boot&amp;nbsp; options and they seem to be at good level when the POR is deasserted. I am getting stuck with this issue and any pointers will be quite helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 10:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342647#M47111</guid>
      <dc:creator>rajniks</dc:creator>
      <dc:date>2014-09-09T10:34:12Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342648#M47112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can check what boot mode is used by processor reading&lt;/P&gt;&lt;P&gt;SRC Boot Mode Register (SRC_SBMR2), SRC_SBMR1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 11:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342648#M47112</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-09T11:54:07Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342649#M47113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to read both registers using lauterbach T32. I am able to see BMOD value changing in the SBMR2 as per my switch settings but SBMR1 remains 0. Is this okay or we are messing something up here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Raj&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 05:18:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342649#M47113</guid>
      <dc:creator>rajniks</dc:creator>
      <dc:date>2014-09-10T05:18:45Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342650#M47114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in serial mode SBMR1 may be not read.&lt;/P&gt;&lt;P&gt;Probably boot signals are connected (shorted) on board internally to smth.&lt;/P&gt;&lt;P&gt;which causes this beahviour. Is it one board only ?&lt;/P&gt;&lt;P&gt;Is it possible to solder board with minimal set of components and check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 10:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342650#M47114</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-10T10:17:40Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342651#M47115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am seeing this behavior on two boards that we have built. I am not suspecting any inadvertent shorts as SBRM2 values changes as per the setting done by the switches. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 11:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342651#M47115</guid>
      <dc:creator>rajniks</dc:creator>
      <dc:date>2014-09-10T11:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342652#M47116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Two boards among what "N" ?&lt;/P&gt;&lt;P&gt;I think you can change processor from good board to&lt;/P&gt;&lt;P&gt;problem board (and vice versa) and check.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 12:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342652#M47116</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-10T12:21:11Z</dc:date>
    </item>
    <item>
      <title>Re: USB Serial Downloader mode - IMX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342653#M47117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Raj, on the off chance you see this, did you ever resolve the issue? We have a custom Dual board and are seeing the exact same behavior. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 18:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Serial-Downloader-mode-IMX6-Quad/m-p/342653#M47117</guid>
      <dc:creator>cameronmadsen</dc:creator>
      <dc:date>2016-05-25T18:34:12Z</dc:date>
    </item>
  </channel>
</rss>