<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Building Image With Yocto - Wrong Kernel Version</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Building-Image-With-Yocto-Wrong-Kernel-Version/m-p/342368#M47036</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks you for updating the post with the answer. I'm sure it will help other users on the community.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Sep 2014 16:02:17 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2014-09-30T16:02:17Z</dc:date>
    <item>
      <title>Building Image With Yocto - Wrong Kernel Version</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-Image-With-Yocto-Wrong-Kernel-Version/m-p/342366#M47034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently trying to build a image for a imx6Q Board. So far I have followed two tutorials&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-94849" title="https://community.freescale.com/docs/DOC-94849"&gt;https://community.freescale.com/docs/DOC-94849&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and the&lt;/P&gt;&lt;P&gt;Freescale Yocto Project's User Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem started when I tried to attach a USB Camera to the board. The board recognizes it, but just as:&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 3 using ci_hdrc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After some google-using I knew I had to load (or at least try to load) the modules "uvcvideo.ko" and/or "gspca_main.ko".&lt;/P&gt;&lt;P&gt;So I tried this on the board&lt;/P&gt;&lt;P&gt;insmod uvcvideo.ko&lt;/P&gt;&lt;P&gt;Which lead to the output:&lt;/P&gt;&lt;P&gt;uvcvideo: disagrees about version of symbol module_layout&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;insmod: ERROR: could not insert module uvcvideo.ko: Invalid module format&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok, the modules where build against a different kernel version - checking the board kernel version (uname -r): 3.16.0-rc3&lt;/P&gt;&lt;P&gt;But the modules reside in the directory /lib/modules/3.10.17-1.0.1_ga+gdac46dc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my question is, where does this kernel 3.16 come from? &lt;/P&gt;&lt;P&gt;At the moment I actually do not care what kernel version I use, I just want to be able to use the modules I build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On a side note: If start menuconfig for virtual/kernel I am able to configure the kernel for 3.10.17.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe someone can help me or point me in the right direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Florian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 14:17:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-Image-With-Yocto-Wrong-Kernel-Version/m-p/342366#M47034</guid>
      <dc:creator>flohg</dc:creator>
      <dc:date>2014-09-24T14:17:02Z</dc:date>
    </item>
    <item>
      <title>Re: Building Image With Yocto - Wrong Kernel Version</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-Image-With-Yocto-Wrong-Kernel-Version/m-p/342367#M47035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found it - somehow the 3.16 kernel was in the nand-flash. I changed the uboot parameters and was able to load the correct kernel from the sdcard. Now I am not able to boot because of some kernel panics, but that is another problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Florian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 06:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-Image-With-Yocto-Wrong-Kernel-Version/m-p/342367#M47035</guid>
      <dc:creator>flohg</dc:creator>
      <dc:date>2014-09-25T06:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: Building Image With Yocto - Wrong Kernel Version</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-Image-With-Yocto-Wrong-Kernel-Version/m-p/342368#M47036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks you for updating the post with the answer. I'm sure it will help other users on the community.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Sep 2014 16:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-Image-With-Yocto-Wrong-Kernel-Version/m-p/342368#M47036</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2014-09-30T16:02:17Z</dc:date>
    </item>
  </channel>
</rss>