<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: HSIC imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HSIC-imx6/m-p/341592#M46940</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;We started from the mentioned file but we apply also the items from Junjie Liu answer.&lt;/P&gt;&lt;P&gt;Even if the file is for Wince, I guess the different steps of initialization for this interface are same even if the implementation differs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you provide exactly what to do to implement the HSIC on H2 ? Have you a code example even if it is not under Linux ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;De : jamesbone &lt;/P&gt;&lt;P&gt;Envoyé : mardi 2 décembre 2014 18:44&lt;/P&gt;&lt;P&gt;À : DAVID Claudette&lt;/P&gt;&lt;P&gt;Objet : Re:  - HSIC imx6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;https://community.freescale.com/&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HSIC imx6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from jamesbone&amp;lt;https://community.freescale.com/people/jamesbone?et=watches.email.thread&amp;gt; in i.MX Community - View the full discussion&amp;lt;https://community.freescale.com/message/459158?et=watches.email.thread#459158&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Dec 2014 08:33:42 GMT</pubDate>
    <dc:creator>cdav</dc:creator>
    <dc:date>2014-12-03T08:33:42Z</dc:date>
    <item>
      <title>HSIC imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HSIC-imx6/m-p/341590#M46938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hi all, I have issue about HSIC link on H2. We follow the method described in &lt;/SPAN&gt;&lt;A class="" data-containerid="-1" data-containertype="-1" data-objectid="251494" data-objecttype="13" href="https://community.freescale.com/servlet/JiveServlet/download/2004-300772-302256-251494/USB_HOST2_initial_settings_in_imx6x.txt.zip"&gt;https://community.freescale.com/servlet/JiveServlet/download/302256-251494/USB_HOST2_initial_settings_in_imx6x.txt.zip&lt;/A&gt;&lt;SPAN&gt; but nothing in ouput. Please, let me know what we have to set exactly to have this link running.Thanks in advance. Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Nov 2014 16:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HSIC-imx6/m-p/341590#M46938</guid>
      <dc:creator>cdav</dc:creator>
      <dc:date>2014-11-14T16:10:10Z</dc:date>
    </item>
    <item>
      <title>Re: HSIC imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HSIC-imx6/m-p/341591#M46939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Claudette,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The file that you mention it was provided by the customer mention that it was not working, if you review the following thread,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/302256"&gt;Need proper initialization for USB Host2 (HSIC) in i.MX6x&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are going to find instructions to add the Host2 support using Linux. But the file it is for WINCE.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 17:43:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HSIC-imx6/m-p/341591#M46939</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-12-02T17:43:31Z</dc:date>
    </item>
    <item>
      <title>Re: HSIC imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HSIC-imx6/m-p/341592#M46940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;We started from the mentioned file but we apply also the items from Junjie Liu answer.&lt;/P&gt;&lt;P&gt;Even if the file is for Wince, I guess the different steps of initialization for this interface are same even if the implementation differs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you provide exactly what to do to implement the HSIC on H2 ? Have you a code example even if it is not under Linux ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;De : jamesbone &lt;/P&gt;&lt;P&gt;Envoyé : mardi 2 décembre 2014 18:44&lt;/P&gt;&lt;P&gt;À : DAVID Claudette&lt;/P&gt;&lt;P&gt;Objet : Re:  - HSIC imx6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;https://community.freescale.com/&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HSIC imx6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from jamesbone&amp;lt;https://community.freescale.com/people/jamesbone?et=watches.email.thread&amp;gt; in i.MX Community - View the full discussion&amp;lt;https://community.freescale.com/message/459158?et=watches.email.thread#459158&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Dec 2014 08:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HSIC-imx6/m-p/341592#M46940</guid>
      <dc:creator>cdav</dc:creator>
      <dc:date>2014-12-03T08:33:42Z</dc:date>
    </item>
  </channel>
</rss>