<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DDR3 Configuration iMx6Q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340981#M46796</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hemanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this seems as hardware issue, one can look at&lt;/P&gt;&lt;P&gt;DDR signals with oscilloscope and check User Guide&lt;/P&gt;&lt;P&gt;Chapter 8 Avoiding Board Bring-up Problems&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Mar 2015 01:45:31 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-03-25T01:45:31Z</dc:date>
    <item>
      <title>DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340978#M46793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are working on a customized board based on iMX6Q sabre lite board. We are trying to initialize the DDR3 and unable to access it via JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We used the DDR Script Aid tool, generated script file for the MT41K256M16HA-125:E DDR3.&amp;nbsp; When we ran the DDR_Stress_Tester_V1.0.3 tool, the stress tool was able to load the code in iRAM (Internal RAM) but after that, it couldn't continue the test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DDR_Stress_Tester reports the error message "Failed to reopen the device". We couldnt find much documentation about this error. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if there is any documentation or any other way to initialize or Test the DDR3 RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 13:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340978#M46793</guid>
      <dc:creator>hemanthkumarven</dc:creator>
      <dc:date>2015-03-23T13:57:11Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340979#M46794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hemanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest to check that JTAG_MOD is grounded.&lt;/P&gt;&lt;P&gt;Also jtag connections are described in Chapter 7&lt;/P&gt;&lt;P&gt;Configuring JTAG Tools &lt;A href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf?fasp=1&amp;amp;WT_TYPE=Users%20Guides&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQ6SDLHDG&lt;/A&gt; &lt;/P&gt;&lt;P&gt;jtag scripts can be found in &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Bare-metal SDK&lt;/P&gt;&lt;P&gt;folder /tools and it may be useful to try simple DDR test /tests/ddr_test.c&lt;/P&gt;&lt;P&gt;with checking signals with oscilloscope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 00:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340979#M46794</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-24T00:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340980#M46795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. JTAG_MOD is grounded and we are able to load the code (DDR test.c) in On chip Ram and Debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the ddr_test.c, while executing "setmem32" command to the DRAM starting address (0x10000000), the execution never returns and the JTAG is unable to halt the target message is displayed if I try to pause the execution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whereas, the same JTAG script and the ddr_test.c works good in the sabrelite board. Based on this, can we conclude this could be a hardware issue rather than a software configuration issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 18:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340980#M46795</guid>
      <dc:creator>hemanthkumarven</dc:creator>
      <dc:date>2015-03-24T18:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340981#M46796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hemanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this seems as hardware issue, one can look at&lt;/P&gt;&lt;P&gt;DDR signals with oscilloscope and check User Guide&lt;/P&gt;&lt;P&gt;Chapter 8 Avoiding Board Bring-up Problems&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 01:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340981#M46796</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-25T01:45:31Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340982#M46797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the sabrelite board, we ran the DDR Stress tester tool V1.0.3 via USB and it ran successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, when we ran the JTAG version, we see the DDR Stress tester tool is not executing after the step where we select the DDR Frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I pause the execution, I could see the disassembly pointing to enter_self_refresh function and it never comes out of this function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached the snapshots for your reference as well. Is there any special setup requirement for JTAG version?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50166i16D9132D05EC889E/image-size/large?v=v2&amp;amp;px=999" title="DDR Stress Test Serial output.png" alt="DDR Stress Test Serial output.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50080iA70542D1FA2BF86B/image-size/large?v=v2&amp;amp;px=999" title="DDR Stress Test Snapshot.png" alt="DDR Stress Test Snapshot.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 12:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340982#M46797</guid>
      <dc:creator>hemanthkumarven</dc:creator>
      <dc:date>2015-03-25T12:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340983#M46798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hemanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;had you checked with oscilloscope DDR signals ?&lt;/P&gt;&lt;P&gt;What is about power lines: DDR, NVCC_DRAM, NVCC_LVDS_2P5 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 12:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340983#M46798</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-25T12:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340984#M46799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick reply. We checked the DDR3 Clock using oscilloscope and we couldnt see any output in DDR3 clock signal in our target board. We are checking the other DDR signals using Oscilloscope in our target/custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the meantime, we ran the DDR stress tool in the sabre lite and observed different behavior when using USB OTG port and JTAG port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to know if there is any setting to run the DDR stress tool properly via JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 12:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340984#M46799</guid>
      <dc:creator>hemanthkumarven</dc:creator>
      <dc:date>2015-03-25T12:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340985#M46800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hemanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are no special settings to run the DDR stress tool via JTAG,&lt;/P&gt;&lt;P&gt;compared with other programs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 01:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340985#M46800</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-26T01:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Configuration iMx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340986#M46801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please try to init DRAM memory via a JTAG script before DDR test running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2015 06:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Configuration-iMx6Q/m-p/340986#M46801</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-08T06:56:35Z</dc:date>
    </item>
  </channel>
</rss>