<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Mouse cursor lost when using MFW_v4lsink in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-cursor-lost-when-using-MFW-v4lsink/m-p/340808#M46762</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We use gstreamer to decode and display video, such as H264, Motion JPEG.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; It works, but I find that the mouse cursor is hidden by video displayed. I notice that totem player can display video with the the same gstreamer plugin mfw_v4lsink, and the mouse cursor is right on the video (not hidden). I have a look at totem source code, there is nothing special, totem just use playbin2 plugin, and does not set any property about the mouse cursor or alpha blending.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; My C program is derive from gst-launch command line as follows, both the program and command line hide the mouse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; gst-launch-0.10 filesrc location=/home/linaro/workspace/234.mp4 ! decodebin2 ! mfw_v4lsink axis-top=0 axis=left=600 disp-width=640 disp-height=480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Why the mouse cursor are hidden by the video displayed, how can I display the cursor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thanks in advence!&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Sep 2014 08:04:03 GMT</pubDate>
    <dc:creator>franklee19731</dc:creator>
    <dc:date>2014-09-24T08:04:03Z</dc:date>
    <item>
      <title>Mouse cursor lost when using MFW_v4lsink</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-cursor-lost-when-using-MFW-v4lsink/m-p/340808#M46762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We use gstreamer to decode and display video, such as H264, Motion JPEG.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; It works, but I find that the mouse cursor is hidden by video displayed. I notice that totem player can display video with the the same gstreamer plugin mfw_v4lsink, and the mouse cursor is right on the video (not hidden). I have a look at totem source code, there is nothing special, totem just use playbin2 plugin, and does not set any property about the mouse cursor or alpha blending.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; My C program is derive from gst-launch command line as follows, both the program and command line hide the mouse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; gst-launch-0.10 filesrc location=/home/linaro/workspace/234.mp4 ! decodebin2 ! mfw_v4lsink axis-top=0 axis=left=600 disp-width=640 disp-height=480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Why the mouse cursor are hidden by the video displayed, how can I display the cursor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thanks in advence!&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 08:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mouse-cursor-lost-when-using-MFW-v4lsink/m-p/340808#M46762</guid>
      <dc:creator>franklee19731</dc:creator>
      <dc:date>2014-09-24T08:04:03Z</dc:date>
    </item>
    <item>
      <title>Re: Mouse cursor lost when using MFW_v4lsink</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-cursor-lost-when-using-MFW-v4lsink/m-p/340809#M46763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What version are you using of BSP?&amp;nbsp; Which board are you using?,&amp;nbsp; I have always seen that the gstreamer gst-launch command always hide the mouse coursor. I think totem player call the Gstreamer command but also do the combining of the cursor with the video. Check this linK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/268425"&gt;i.MX53 gstreamer on framebuffer?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 16:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mouse-cursor-lost-when-using-MFW-v4lsink/m-p/340809#M46763</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-10-02T16:23:03Z</dc:date>
    </item>
  </channel>
</rss>