<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: External clock on RGMII_TX_CTL possible for RMII?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/External-clock-on-RGMII-TX-CTL-possible-for-RMII/m-p/340108#M46571</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Magnus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this signal also can be used for RMII as described in&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6SDLRM&lt;/A&gt; Table 23-1. ENET External Signals&lt;/P&gt;&lt;P&gt;There are some RMII examples below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/313741"&gt;RMII on i.MX6 (L3.0.35_4.1.0)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/346089"&gt;Re: RMII interface on i.MX6 Solo&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Dec 2014 00:33:28 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-12-11T00:33:28Z</dc:date>
    <item>
      <title>External clock on RGMII_TX_CTL possible for RMII?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-clock-on-RGMII-TX-CTL-possible-for-RMII/m-p/340107#M46570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom IMXDL board with a KSZ8863 switch.&lt;/P&gt;&lt;P&gt;According to MDIO the switch is fine, but RMII is dead silent.&lt;/P&gt;&lt;P&gt;Both IMXDL and PHY are clocked by external clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to confirm that it is indeed possible to use RGMII_TX_CTL to clock RMII from an external clock?&lt;/P&gt;&lt;P&gt;The HW dev. guide (IMX6DQ6SDLHDG) is a bit light on detail regarding RGMII_TX_CTL, as GPIO_16 is the recommended external clock sink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If RGMII_TX_CTL is a valid clock sink for RMII, it's a SW issue and I'd much appreciate any sample code.&lt;/P&gt;&lt;P&gt;I'm trying to get ethernet running on uboot, for a start.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2014 16:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-clock-on-RGMII-TX-CTL-possible-for-RMII/m-p/340107#M46570</guid>
      <dc:creator>MagnusNilsson</dc:creator>
      <dc:date>2014-12-10T16:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: External clock on RGMII_TX_CTL possible for RMII?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-clock-on-RGMII-TX-CTL-possible-for-RMII/m-p/340108#M46571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Magnus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this signal also can be used for RMII as described in&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6SDLRM&lt;/A&gt; Table 23-1. ENET External Signals&lt;/P&gt;&lt;P&gt;There are some RMII examples below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/313741"&gt;RMII on i.MX6 (L3.0.35_4.1.0)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/346089"&gt;Re: RMII interface on i.MX6 Solo&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Dec 2014 00:33:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-clock-on-RGMII-TX-CTL-possible-for-RMII/m-p/340108#M46571</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-11T00:33:28Z</dc:date>
    </item>
  </channel>
</rss>