<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDisplay type and resolution (for video/graphic/display issues)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-type-and-resolution-for-video-graphic-display-issues/m-p/339374#M46384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45050i1D26AA0B32CA3820/image-size/large?v=v2&amp;amp;px=999" title="colorbanding1.jpg" alt="colorbanding1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on infotainment system and developing HMI also for it. the configuration is SABRE SD&amp;nbsp; with Linaro 11.10.&lt;/P&gt;&lt;P&gt;colors used are RGB888.&lt;/P&gt;&lt;P&gt;We are noticing image distortion; as shown in attached image.&lt;/P&gt;&lt;P&gt;galcore module is also available on system.&lt;/P&gt;&lt;P&gt;Is this a settings issue; or is there any way to enable/disable graphics acceleration in LINARO 11.10 working SABRE SD. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Sep 2014 13:46:41 GMT</pubDate>
    <dc:creator>jitendramaharsh</dc:creator>
    <dc:date>2014-09-04T13:46:41Z</dc:date>
    <item>
      <title>Display type and resolution (for video/graphic/display issues)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-type-and-resolution-for-video-graphic-display-issues/m-p/339374#M46384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45050i1D26AA0B32CA3820/image-size/large?v=v2&amp;amp;px=999" title="colorbanding1.jpg" alt="colorbanding1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on infotainment system and developing HMI also for it. the configuration is SABRE SD&amp;nbsp; with Linaro 11.10.&lt;/P&gt;&lt;P&gt;colors used are RGB888.&lt;/P&gt;&lt;P&gt;We are noticing image distortion; as shown in attached image.&lt;/P&gt;&lt;P&gt;galcore module is also available on system.&lt;/P&gt;&lt;P&gt;Is this a settings issue; or is there any way to enable/disable graphics acceleration in LINARO 11.10 working SABRE SD. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Sep 2014 13:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-type-and-resolution-for-video-graphic-display-issues/m-p/339374#M46384</guid>
      <dc:creator>jitendramaharsh</dc:creator>
      <dc:date>2014-09-04T13:46:41Z</dc:date>
    </item>
    <item>
      <title>Re: Display type and resolution (for video/graphic/display issues)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-type-and-resolution-for-video-graphic-display-issues/m-p/339375#M46385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Previous posts should help in your settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/308582"&gt;IMX6q GPU driver, galcore does not load&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95185"&gt;How to create ubuntu hardfloat rootfs for imx6d/q&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/307061"&gt;Want to try hard float vivante drivers for MX6?&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 14:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-type-and-resolution-for-video-graphic-display-issues/m-p/339375#M46385</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2014-09-17T14:30:41Z</dc:date>
    </item>
  </channel>
</rss>