<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to Select The SION Bit in Different Conditions?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Select-The-SION-Bit-in-Different-Conditions/m-p/338133#M46184</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SW Loopback (SION) – the SION bit (SW Input On in IOMUXC_SW_MUX_CTL) &lt;/P&gt;&lt;P&gt;override the regular PAD functionality and forces the input path to &lt;/P&gt;&lt;P&gt;be active regardless of the value driven by the corresponding &lt;/P&gt;&lt;P&gt;module. It can be used for:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Loop Back - Module X drives the PAD and also receive PAD value as an &lt;/P&gt;&lt;P&gt;input. Required by I2C,SDHC modules.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GPIO Capture - Module X drives the PAD and the value is captured by GPIO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Loop Back to module Y - Module X drives the PAD and module Y also receives &lt;/P&gt;&lt;P&gt;PAD value as an input. This can be used for driving module Y input without &lt;/P&gt;&lt;P&gt;connecting a real device on board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Mar 2015 03:52:31 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-03-23T03:52:31Z</dc:date>
    <item>
      <title>How to Select The SION Bit in Different Conditions?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Select-The-SION-Bit-in-Different-Conditions/m-p/338132#M46183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Maybe I dont know how to use the SION Bit, could you tell me what conditons do we need to set SION bit? please give me an example,3Q~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 00:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Select-The-SION-Bit-in-Different-Conditions/m-p/338132#M46183</guid>
      <dc:creator>tony_l_cai</dc:creator>
      <dc:date>2015-03-23T00:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: How to Select The SION Bit in Different Conditions?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Select-The-SION-Bit-in-Different-Conditions/m-p/338133#M46184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SW Loopback (SION) – the SION bit (SW Input On in IOMUXC_SW_MUX_CTL) &lt;/P&gt;&lt;P&gt;override the regular PAD functionality and forces the input path to &lt;/P&gt;&lt;P&gt;be active regardless of the value driven by the corresponding &lt;/P&gt;&lt;P&gt;module. It can be used for:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Loop Back - Module X drives the PAD and also receive PAD value as an &lt;/P&gt;&lt;P&gt;input. Required by I2C,SDHC modules.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GPIO Capture - Module X drives the PAD and the value is captured by GPIO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Loop Back to module Y - Module X drives the PAD and module Y also receives &lt;/P&gt;&lt;P&gt;PAD value as an input. This can be used for driving module Y input without &lt;/P&gt;&lt;P&gt;connecting a real device on board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 03:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Select-The-SION-Bit-in-Different-Conditions/m-p/338133#M46184</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-23T03:52:31Z</dc:date>
    </item>
  </channel>
</rss>