<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestion, i.MX28 GPMI for AsyncRAM/Nor Flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-GPMI-for-AsyncRAM-Nor-Flash/m-p/337936#M46146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about GPMI of i.MX28.&lt;/P&gt;&lt;P&gt;My customer wants to use GPMI port of i.MX28 for connecting Async RAM or Nor Flash.&lt;/P&gt;&lt;P&gt;They want that even if the external circuitry should be needed.&lt;/P&gt;&lt;P&gt;(1)&amp;nbsp; Can the GPMI port be configured as not output NAND command?&lt;/P&gt;&lt;P&gt;If not, they think it needs the external circuitry for gating the NAND command output by using CLE signal.&lt;/P&gt;&lt;P&gt;(2) Can i.MX28 control fully the address output from GPMI port?&lt;/P&gt;&lt;P&gt;To handle address output to external RAM/NOR, the external circuitry may need to latch Row Adr3. Then 8bit address space can be controlled by i.MX28.&lt;/P&gt;&lt;P&gt;Can i.MX28 software specify the Row Adr3 fully?&lt;/P&gt;&lt;P&gt;(3) Reading data from Async RAM/Nor Flash&lt;/P&gt;&lt;P&gt;The data transfer of NAND can be seen as a kind of burst transfer. To accessing AsyncRAM/Nor, only the first data(or 2nd data) is needed.&lt;/P&gt;&lt;P&gt;Do you have any ideas how to handle the read/write data by CPU?&lt;/P&gt;&lt;P&gt;(4) Do you have any examples on the ideas to connect AsyncRAM/Nor to GPMI ports?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 01 Feb 2015 13:25:30 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-02-01T13:25:30Z</dc:date>
    <item>
      <title>Question, i.MX28 GPMI for AsyncRAM/Nor Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-GPMI-for-AsyncRAM-Nor-Flash/m-p/337936#M46146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about GPMI of i.MX28.&lt;/P&gt;&lt;P&gt;My customer wants to use GPMI port of i.MX28 for connecting Async RAM or Nor Flash.&lt;/P&gt;&lt;P&gt;They want that even if the external circuitry should be needed.&lt;/P&gt;&lt;P&gt;(1)&amp;nbsp; Can the GPMI port be configured as not output NAND command?&lt;/P&gt;&lt;P&gt;If not, they think it needs the external circuitry for gating the NAND command output by using CLE signal.&lt;/P&gt;&lt;P&gt;(2) Can i.MX28 control fully the address output from GPMI port?&lt;/P&gt;&lt;P&gt;To handle address output to external RAM/NOR, the external circuitry may need to latch Row Adr3. Then 8bit address space can be controlled by i.MX28.&lt;/P&gt;&lt;P&gt;Can i.MX28 software specify the Row Adr3 fully?&lt;/P&gt;&lt;P&gt;(3) Reading data from Async RAM/Nor Flash&lt;/P&gt;&lt;P&gt;The data transfer of NAND can be seen as a kind of burst transfer. To accessing AsyncRAM/Nor, only the first data(or 2nd data) is needed.&lt;/P&gt;&lt;P&gt;Do you have any ideas how to handle the read/write data by CPU?&lt;/P&gt;&lt;P&gt;(4) Do you have any examples on the ideas to connect AsyncRAM/Nor to GPMI ports?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Feb 2015 13:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-GPMI-for-AsyncRAM-Nor-Flash/m-p/337936#M46146</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-02-01T13:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX28 GPMI for AsyncRAM/Nor Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-GPMI-for-AsyncRAM-Nor-Flash/m-p/337937#M46147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; The GPMI of the i.MX28 supports only NAND devices. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;It is not intended to work with other devices, such as &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Async RAM or Nor Flash. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 07:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-GPMI-for-AsyncRAM-Nor-Flash/m-p/337937#M46147</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-02-02T07:13:01Z</dc:date>
    </item>
  </channel>
</rss>