<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic u-boot compilation error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-compilation-error/m-p/337026#M45989</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm following for this manual &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/README?h=daisy_3.10.53-1.1.0_GA" title="http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/README?h=daisy_3.10.53-1.1.0_GA"&gt;meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;repo sync&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Building X11&lt;BR /&gt;------------&lt;BR /&gt;MACHINE=wandboard-dual source fsl-setup-release.sh -b build-x11 -e x11&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;bitbake fsl-image-qt5&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I got error on clean source:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;| arch/arm/imx-common/built-in.o: In function `arch_preboot_os':&lt;/P&gt;&lt;P&gt;| /home/x0158990/work/os/fsl-arm-yocto-bsp/build-X11/tmp/work/wandboard_dual-poky-linux-gnueabi/u-boot-imx/2014.04-r0/git/arch/arm/imx-common/cpu.c:203: undefined reference to `ldo_mode_set'&lt;/P&gt;&lt;P&gt;| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/x0158990/work/os/fsl-arm-yocto-bsp/build-X11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696&lt;/P&gt;&lt;P&gt;| arm-poky-linux-gnueabi-ld.bfd: error: required section '.rel.plt' not found in the linker script&lt;/P&gt;&lt;P&gt;| arm-poky-linux-gnueabi-ld.bfd: final link failed: Invalid operation&lt;/P&gt;&lt;P&gt;| make: *** [u-boot] Error 1&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_compile (log file is located at /home/x0158990/work/os/fsl-arm-yocto-bsp/build-X11/tmp/work/wandboard_dual-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.8980)&lt;/P&gt;&lt;P&gt;ERROR: Task 234 (/home/x0158990/work/os/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 4851 tasks of which 4821 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Jan 2015 16:49:05 GMT</pubDate>
    <dc:creator>volodymyrmakhit</dc:creator>
    <dc:date>2015-01-12T16:49:05Z</dc:date>
    <item>
      <title>u-boot compilation error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-compilation-error/m-p/337026#M45989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm following for this manual &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/README?h=daisy_3.10.53-1.1.0_GA" title="http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/README?h=daisy_3.10.53-1.1.0_GA"&gt;meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;repo sync&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Building X11&lt;BR /&gt;------------&lt;BR /&gt;MACHINE=wandboard-dual source fsl-setup-release.sh -b build-x11 -e x11&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;bitbake fsl-image-qt5&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I got error on clean source:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;| arch/arm/imx-common/built-in.o: In function `arch_preboot_os':&lt;/P&gt;&lt;P&gt;| /home/x0158990/work/os/fsl-arm-yocto-bsp/build-X11/tmp/work/wandboard_dual-poky-linux-gnueabi/u-boot-imx/2014.04-r0/git/arch/arm/imx-common/cpu.c:203: undefined reference to `ldo_mode_set'&lt;/P&gt;&lt;P&gt;| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/x0158990/work/os/fsl-arm-yocto-bsp/build-X11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696&lt;/P&gt;&lt;P&gt;| arm-poky-linux-gnueabi-ld.bfd: error: required section '.rel.plt' not found in the linker script&lt;/P&gt;&lt;P&gt;| arm-poky-linux-gnueabi-ld.bfd: final link failed: Invalid operation&lt;/P&gt;&lt;P&gt;| make: *** [u-boot] Error 1&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_compile (log file is located at /home/x0158990/work/os/fsl-arm-yocto-bsp/build-X11/tmp/work/wandboard_dual-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.8980)&lt;/P&gt;&lt;P&gt;ERROR: Task 234 (/home/x0158990/work/os/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 4851 tasks of which 4821 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jan 2015 16:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-compilation-error/m-p/337026#M45989</guid>
      <dc:creator>volodymyrmakhit</dc:creator>
      <dc:date>2015-01-12T16:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot compilation error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-compilation-error/m-p/337027#M45990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are using our FSL official release. Therefore the wandboard machine is not expected to work with this branch &lt;CODE&gt; imx-3.10.53-1.1.0_ga&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;I suggest you to try the below one for the wandboard&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;repo init -u &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://github.com/Freescale/fsl-community-bsp-platform" target="_blank"&gt;https://github.com/Freescale/fsl-community-bsp-platform&lt;/A&gt;&lt;SPAN&gt; -b dizzy&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 17:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-compilation-error/m-p/337027#M45990</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-01-13T17:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot compilation error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-compilation-error/m-p/337028#M45991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi alejan,&lt;/P&gt;&lt;P&gt;when I build my 3.14.52_1.1.0_ga uboot, I got below error.The config I used is&amp;nbsp;wandboard_dl_defconfig just under the configs. Can you give some comments how can I fix this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;drivers/built-in.o: In function `imx_thermal_probe':&lt;BR /&gt;/home/lucid/imx6dl/uboot-imx-rel_imx_3.14.52_1.1.0_ga/drivers/thermal/imx_thermal.c:226: undefined reference to `dev_get_platdata'&lt;BR /&gt;/home/lucid/imx6dl/uboot-imx-rel_imx_3.14.52_1.1.0_ga/drivers/thermal/imx_thermal.c:227: undefined reference to `dev_get_priv'&lt;BR /&gt;arm-linux-gnueabihf-ld.bfd: BFD (GNU Binutils for Ubuntu) 2.24 assertion fail ../../bfd/elf32-arm.c:7696&lt;BR /&gt;arm-linux-gnueabihf-ld.bfd: BFD (GNU Binutils for Ubuntu) 2.24 assertion fail ../../bfd/elf32-arm.c:7696&lt;BR /&gt;arm-linux-gnueabihf-ld.bfd: BFD (GNU Binutils for Ubuntu) 2.24 assertion fail ../../bfd/elf32-arm.c:7696&lt;BR /&gt;arm-linux-gnueabihf-ld.bfd: BFD (GNU Binutils for Ubuntu) 2.24 assertion fail ../../bfd/elf32-arm.c:7696&lt;BR /&gt;arm-linux-gnueabihf-ld.bfd: BFD (GNU Binutils for Ubuntu) 2.24 assertion fail ../../bfd/elf32-arm.c:7696&lt;BR /&gt;arm-linux-gnueabihf-ld.bfd: error: required section '.rel.plt' not found in the linker script&lt;BR /&gt;arm-linux-gnueabihf-ld.bfd: final link failed: Invalid operation&lt;BR /&gt;make: *** [u-boot] Error 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Wenming&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 12:11:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-compilation-error/m-p/337028#M45991</guid>
      <dc:creator>wenmingfeng</dc:creator>
      <dc:date>2016-12-05T12:11:46Z</dc:date>
    </item>
  </channel>
</rss>