<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: CAN Bit rate calculation for IMX6 solo processor</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Bit-rate-calculation-for-IMX6-solo-processor/m-p/336862#M45968</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are more than one configurations that can achieve the 33.33KHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bit time can be composed of 8 to 25 time quata.&lt;/P&gt;&lt;P&gt;Lets assume that you choose a bit time of 25 time quanta. That means that each quantum should be 25*33.33KHz.&lt;/P&gt;&lt;P&gt;To ahieve that frequency with a 30MHz clock you need a prescaler = 30MHz/(25 * 33.33KHz) = 36.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore the TIME SEGMENT 1 = 16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TIME SEGMENT&amp;nbsp; 2 =&amp;nbsp; 8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With this you can choose the correct values for PROP_SEG, PSEG and PSEG2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I hope that helps,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Nov 2014 16:50:27 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2014-11-18T16:50:27Z</dc:date>
    <item>
      <title>CAN Bit rate calculation for IMX6 solo processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Bit-rate-calculation-for-IMX6-solo-processor/m-p/336861#M45967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to get the register values for custom bit rate.&lt;/P&gt;&lt;P&gt;I used below link to generate register values for bit rate calculation for other bit rate settings (standard bit rate settings)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.bittiming.can-wiki.info/"&gt;http://www.bittiming.can-wiki.info/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Used Freescale flexCAN option for the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now i want to generate register values for to 33.33Khz with the system is clocked at 30Mhz.&lt;/P&gt;&lt;P&gt;Any help on generating the register values for the same or share the procedure to generate one will be appreciated&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Shyam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Nov 2014 13:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-Bit-rate-calculation-for-IMX6-solo-processor/m-p/336861#M45967</guid>
      <dc:creator>shyam</dc:creator>
      <dc:date>2014-11-13T13:04:27Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Bit rate calculation for IMX6 solo processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Bit-rate-calculation-for-IMX6-solo-processor/m-p/336862#M45968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are more than one configurations that can achieve the 33.33KHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bit time can be composed of 8 to 25 time quata.&lt;/P&gt;&lt;P&gt;Lets assume that you choose a bit time of 25 time quanta. That means that each quantum should be 25*33.33KHz.&lt;/P&gt;&lt;P&gt;To ahieve that frequency with a 30MHz clock you need a prescaler = 30MHz/(25 * 33.33KHz) = 36.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore the TIME SEGMENT 1 = 16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TIME SEGMENT&amp;nbsp; 2 =&amp;nbsp; 8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With this you can choose the correct values for PROP_SEG, PSEG and PSEG2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I hope that helps,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 16:50:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-Bit-rate-calculation-for-IMX6-solo-processor/m-p/336862#M45968</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-11-18T16:50:27Z</dc:date>
    </item>
  </channel>
</rss>