<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wrong image format for bootm command kernel image not found android in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336379#M45786</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to Android user guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boot from SD card&lt;/P&gt;&lt;P&gt;Change the board boot switch to MMC2 (SD3) boot: (SW6) 01000010 (from 1-8 bit). To clear the bootargs env and set up&lt;/P&gt;&lt;P&gt;the booting from SD card in SD slot 3, you can use the following command:&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; setenv fastboot_dev mmc2 [eMMC as fastboot deivce]&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; setenv bootcmd booti mmc2 [Load the boot.img from SD card]&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32&lt;/P&gt;&lt;P&gt;video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M&lt;/P&gt;&lt;P&gt;androidboot.console=ttymxc0 androidboot.hardware=freescale #[Optional]&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; saveenv #[Save the environments]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Feb 2015 09:11:38 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2015-02-25T09:11:38Z</dc:date>
    <item>
      <title>Wrong image format for bootm command kernel image not found android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336376#M45783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am newbie trying to port the default android image(4.4.2) onto imx6 dual lite auto board . I successfully flashed the image onto sdcard media by following the quick start guide . Bu t when I enter into U boot it says " Wrong image format for bootm command Error : Kernel image not found". Can somebody help me with this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bootargs=console=ttymxc3,115200 rdinit=/linuxrc&lt;/P&gt;&lt;P&gt;bootcmd=bootm 0x10800000 0x10c00000&lt;/P&gt;&lt;P&gt;bootdelay=0&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;ipaddr=192.168.1.103&lt;/P&gt;&lt;P&gt;serverip=192.168.1.101&lt;/P&gt;&lt;P&gt;netmask=255.255.255.0&lt;/P&gt;&lt;P&gt;loadaddr=0x10800000&lt;/P&gt;&lt;P&gt;rd_loadaddr=(0x10800000 + 0x300000)&lt;/P&gt;&lt;P&gt;netdev=eth0&lt;/P&gt;&lt;P&gt;ethprime=FEC0&lt;/P&gt;&lt;P&gt;uboot=u-boot.bin&lt;/P&gt;&lt;P&gt;kernel=uImage&lt;/P&gt;&lt;P&gt;stdin=serial&lt;/P&gt;&lt;P&gt;stdout=serial&lt;/P&gt;&lt;P&gt;stderr=serial&lt;/P&gt;&lt;P&gt;ethact=FEC0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 07:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336376#M45783</guid>
      <dc:creator>arunswarnam</dc:creator>
      <dc:date>2015-02-25T07:16:04Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong image format for bootm command kernel image not found android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336377#M45784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can you set following&lt;/P&gt;&lt;P&gt;setenv bootcmd booti mmc2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 08:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336377#M45784</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2015-02-25T08:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong image format for bootm command kernel image not found android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336378#M45785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have set that . But then when I try to boot it says ""booti mmc2 not found""&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6SDL ARM2-MFG U-Boot &amp;gt; printenv&lt;/P&gt;&lt;P&gt;bootdelay=0&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;ipaddr=192.168.1.103&lt;/P&gt;&lt;P&gt;serverip=192.168.1.101&lt;/P&gt;&lt;P&gt;netmask=255.255.255.0&lt;/P&gt;&lt;P&gt;loadaddr=0x10800000&lt;/P&gt;&lt;P&gt;rd_loadaddr=(0x10800000 + 0x300000)&lt;/P&gt;&lt;P&gt;netdev=eth0&lt;/P&gt;&lt;P&gt;ethprime=FEC0&lt;/P&gt;&lt;P&gt;uboot=u-boot.bin&lt;/P&gt;&lt;P&gt;kernel=uImage&lt;/P&gt;&lt;P&gt;stdin=serial&lt;/P&gt;&lt;P&gt;stdout=serial&lt;/P&gt;&lt;P&gt;stderr=serial&lt;/P&gt;&lt;P&gt;ethact=FEC0&lt;/P&gt;&lt;P&gt;bootargs=console=ttymxc3,115200 androidboot.console=ttymxc3 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=28M androidboot.hardware=freescale&lt;/P&gt;&lt;P&gt;bootcmd=booti mmc2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 480/8188 bytes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 08:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336378#M45785</guid>
      <dc:creator>arunswarnam</dc:creator>
      <dc:date>2015-02-25T08:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong image format for bootm command kernel image not found android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336379#M45786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to Android user guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boot from SD card&lt;/P&gt;&lt;P&gt;Change the board boot switch to MMC2 (SD3) boot: (SW6) 01000010 (from 1-8 bit). To clear the bootargs env and set up&lt;/P&gt;&lt;P&gt;the booting from SD card in SD slot 3, you can use the following command:&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; setenv fastboot_dev mmc2 [eMMC as fastboot deivce]&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; setenv bootcmd booti mmc2 [Load the boot.img from SD card]&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32&lt;/P&gt;&lt;P&gt;video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M&lt;/P&gt;&lt;P&gt;androidboot.console=ttymxc0 androidboot.hardware=freescale #[Optional]&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; saveenv #[Save the environments]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 09:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336379#M45786</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2015-02-25T09:11:38Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong image format for bootm command kernel image not found android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336380#M45787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using sabre AI board . I couldnt find Sw6&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 10:56:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336380#M45787</guid>
      <dc:creator>arunswarnam</dc:creator>
      <dc:date>2015-02-25T10:56:44Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong image format for bootm command kernel image not found android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336381#M45788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I fixed this issue .Though not very sure of the answer&amp;nbsp; few things I found was&lt;/P&gt;&lt;P&gt;1) Put the proper .bin file for the corresponding board and add only full image files and not the core image files for flashing onto the media as specified in the android quick start guide.&lt;/P&gt;&lt;P&gt;2) The cfg file should be properly configured by following the board and name values as specified in the user guide and set the chip value to MX6DL LINUX UPDATE .&lt;/P&gt;&lt;P&gt;For sabre AI Imx6 Dual LIte board &amp;amp; SD card media this is the cfg file content &lt;/P&gt;&lt;P&gt;[profiles]&lt;/P&gt;&lt;P&gt;chip = MX6DL Linux Update&lt;/P&gt;&lt;P&gt;[platform]&lt;/P&gt;&lt;P&gt;board = SabreAuto&lt;/P&gt;&lt;P&gt;[LIST]&lt;/P&gt;&lt;P&gt;name = Android-MX6DL-SabreAuto-SD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 14:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wrong-image-format-for-bootm-command-kernel-image-not-found/m-p/336381#M45788</guid>
      <dc:creator>arunswarnam</dc:creator>
      <dc:date>2015-02-25T14:03:23Z</dc:date>
    </item>
  </channel>
</rss>