<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX53 NAND  NFC Kernel support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336215#M45755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OK. It looks like &lt;SPAN class="line"&gt;CONFIG_MTD_NAND_MXC_V3=y is the correct configuration option to use the iMX53 NAND Flash Controller.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;I'm just curious what &lt;SPAN class="line"&gt;CONFIG_MTD_NAND_IMX_NFC&amp;nbsp; is used for?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="line"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="line"&gt;Bruno&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Feb 2015 09:59:23 GMT</pubDate>
    <dc:creator>bdp42</dc:creator>
    <dc:date>2015-02-02T09:59:23Z</dc:date>
    <item>
      <title>iMX53 NAND  NFC Kernel support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336213#M45753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a simple question about the correct kernel config option for iMX53 NAND NFC support. Should CONFIG_MTD_NAND_IMX_NFC should be enabled in the kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason I ask is that the imx5_defconfig file (which supports MX53 NAND) does not have it set yet it looks like it should be set. Here's the relevant piece of the config file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;#&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# Disk-On-Chip Device Drivers&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;#&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_DOC2000 is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_DOC2001 is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_DOC2001PLUS is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;CONFIG_MTD_NAND=y&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_VERIFY_WRITE is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_ECC_SMC is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_MUSEUM_IDS is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_GPIO is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;CONFIG_MTD_NAND_IDS=y&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_DISKONCHIP is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_NANDSIM is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_IMX_NFC is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;CONFIG_MTD_NAND_MXC_V3=y&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_MXC_SWECC is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_MXC_FORCE_CE is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MXC_NAND_LOW_LEVEL_ERASE is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_NAND_PLATFORM is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_ALAUDA is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class="line"&gt;# CONFIG_MTD_ONENAND is not set&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone clarify this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 17:22:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336213#M45753</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-01-30T17:22:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 NAND  NFC Kernel support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336214#M45754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe not since one has already &lt;SPAN class="line"&gt;CONFIG_MTD_NAND_MXC_V3=y,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;also refer to attached file. In ltib build one can select ard board,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;it has nand support&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_11.05_ER_SOURCE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Linux 2.6.35 Source Code Files and documentation 11.05 for i.MX53 SABRE Tablet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Jan 2015 00:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336214#M45754</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-31T00:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 NAND  NFC Kernel support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336215#M45755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OK. It looks like &lt;SPAN class="line"&gt;CONFIG_MTD_NAND_MXC_V3=y is the correct configuration option to use the iMX53 NAND Flash Controller.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;I'm just curious what &lt;SPAN class="line"&gt;CONFIG_MTD_NAND_IMX_NFC&amp;nbsp; is used for?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="line"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="line"&gt;Bruno&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 09:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336215#M45755</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-02-02T09:59:23Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 NAND  NFC Kernel support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336216#M45756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="line"&gt;CONFIG_MTD_NAND_IMX_NFC was&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="line"&gt;for older NFC revisions used in i.MX21,MX31.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="line"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 10:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-NAND-NFC-Kernel-support/m-p/336216#M45756</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-02-02T10:03:31Z</dc:date>
    </item>
  </channel>
</rss>