<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Sabre board power sources bad sizing?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335884#M45641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3920 mA is for very special test "Power Virus", not practically&lt;/P&gt;&lt;P&gt;achieved in real life applications. Real power consumption figures&lt;/P&gt;&lt;P&gt;one can find in &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4509&lt;/A&gt; i.MX 6Dual/6Quad Power Consumption Measurement.&lt;/P&gt;&lt;P&gt;However in general you are right, pmic current limit should not be exceed,&lt;/P&gt;&lt;P&gt;otherwise processor could not work properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Mar 2015 13:07:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-03-21T13:07:40Z</dc:date>
    <item>
      <title>Sabre board power sources bad sizing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335883#M45640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with the SABRE Platform for Smart Devices Reference Design Based on the i.MX 6 quad core. I have noticed that the power consumption of the IMX6 core (VDD_ARM23_IN) may be grater than the used source capability, i.e. the switching regulator PF0100 SW1A/B can generate just up to 2500 mA and the ARMCORE could achieve a consumption up to&amp;nbsp; 3920 mA. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is true, the SABRE board would work ok if this limit is not exceed. However, if the IMX6 is bring under a high performance processing task, it could not work properly. &lt;SPAN style="font-size: 13.3333330154419px;"&gt;Am I right? or Am I forgetting something? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2015 16:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335883#M45640</guid>
      <dc:creator>markoslosada</dc:creator>
      <dc:date>2015-03-20T16:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: Sabre board power sources bad sizing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335884#M45641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3920 mA is for very special test "Power Virus", not practically&lt;/P&gt;&lt;P&gt;achieved in real life applications. Real power consumption figures&lt;/P&gt;&lt;P&gt;one can find in &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4509&lt;/A&gt; i.MX 6Dual/6Quad Power Consumption Measurement.&lt;/P&gt;&lt;P&gt;However in general you are right, pmic current limit should not be exceed,&lt;/P&gt;&lt;P&gt;otherwise processor could not work properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Mar 2015 13:07:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335884#M45641</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-21T13:07:40Z</dc:date>
    </item>
    <item>
      <title>Re: Sabre board power sources bad sizing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335885#M45642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How long does the power virus last? Is this for a short period of time?&lt;/P&gt;&lt;P&gt;Could you confirm that as long as the PMIC current limit is not hit, the virus mode can be achieved?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any measurement results for virus mode done on PF0100 ? It will be extremely useful for our upcoming PMIC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Adrien&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;adding &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/christianassier"&gt;christianassier&lt;/A&gt;​;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mohamedzubair"&gt;mohamedzubair&lt;/A&gt;​;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/AnandBalakrishnan"&gt;AnandBalakrishnan&lt;/A&gt;​;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 18:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335885#M45642</guid>
      <dc:creator>adriengambino</dc:creator>
      <dc:date>2015-05-29T18:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: Sabre board power sources bad sizing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335886#M45643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;power virus codes are internal codes, not available&lt;/P&gt;&lt;P&gt;for customers. AN4509 shows data for real life&lt;/P&gt;&lt;P&gt;applications, please use them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 May 2015 14:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-board-power-sources-bad-sizing/m-p/335886#M45643</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-05-30T14:36:12Z</dc:date>
    </item>
  </channel>
</rss>