<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: hardware based video decoder example for freescale i-max6 dual processor. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/hardware-based-video-decoder-example-for-freescale-i-max6-dual/m-p/335859#M45628</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Safraz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use gplay or imx-test package included in ltib (mxc_vpu_test):&lt;/P&gt;&lt;P&gt;./mxc_vpu_test.out -D "-i /usr/vectors/file.mjpg -f 7" &lt;/P&gt;&lt;P&gt;Note that mxc_vpu_test can only play RAW video files.&lt;/P&gt;&lt;P&gt;Also next link may be useful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/374103"&gt;JPEG hardware decode and resize in i.MX6&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jan 2015 01:00:50 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-13T01:00:50Z</dc:date>
    <item>
      <title>hardware based video decoder example for freescale i-max6 dual processor.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hardware-based-video-decoder-example-for-freescale-i-max6-dual/m-p/335858#M45627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a working example for hardware based video decoder for MJPG stream for i-max6 dual processor. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jan 2015 12:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hardware-based-video-decoder-example-for-freescale-i-max6-dual/m-p/335858#M45627</guid>
      <dc:creator>sarfrazahmed07</dc:creator>
      <dc:date>2015-01-12T12:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: hardware based video decoder example for freescale i-max6 dual processor.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hardware-based-video-decoder-example-for-freescale-i-max6-dual/m-p/335859#M45628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Safraz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use gplay or imx-test package included in ltib (mxc_vpu_test):&lt;/P&gt;&lt;P&gt;./mxc_vpu_test.out -D "-i /usr/vectors/file.mjpg -f 7" &lt;/P&gt;&lt;P&gt;Note that mxc_vpu_test can only play RAW video files.&lt;/P&gt;&lt;P&gt;Also next link may be useful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/374103"&gt;JPEG hardware decode and resize in i.MX6&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 01:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hardware-based-video-decoder-example-for-freescale-i-max6-dual/m-p/335859#M45628</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-13T01:00:50Z</dc:date>
    </item>
  </channel>
</rss>