<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6SDL CLKO support range. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335836#M45624</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes correct, main purpose is for test.&lt;/P&gt;&lt;P&gt;It also can be used for other purposes, provided&lt;/P&gt;&lt;P&gt;that one carefully design hard&amp;amp;software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Dec 2014 13:44:52 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-12-10T13:44:52Z</dc:date>
    <item>
      <title>i.MX6SDL CLKO support range.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335833#M45621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our partner have a question about i.MX6SDL CCM.&lt;/P&gt;&lt;P&gt;Please see CCM_CLK_SRC_DIV description in Table 18-1 of IMX6SDLRM Rev.1.&lt;/P&gt;&lt;P&gt;It says "These output clocks are connected to the pads and can provide support for testing."&lt;/P&gt;&lt;P&gt;Then, they want to confirm the meaning of "can provide support for testing".&lt;/P&gt;&lt;P&gt;Can freescale guarantee the CLKO output for test only?&lt;/P&gt;&lt;P&gt;Or can freescale guarantee the output for any usage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, they are using CLKO2 for audio master clock on their custom board, but sometimes CLKO output stops.&lt;/P&gt;&lt;P&gt;So they want to confirm the support range of CLKO at first whether freescale can support their usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2014 11:39:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335833#M45621</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-12-09T11:39:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL CLKO support range.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335834#M45622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right: formally speaking these signals are for testing, also&lt;/P&gt;&lt;P&gt;there are parameters for them in Datasheet. From Table 18-1. CCM Sub-blocks &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6SDLRM&lt;/A&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;..two output clocks, CCM_CLKO1 and CCM_CLKO2, for observability.&lt;/P&gt;&lt;P&gt;These output clocks are connected to the pads and can provide support for testing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2014 11:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335834#M45622</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-09T11:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL CLKO support range.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335835#M45623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Excuse me, which is correct?&lt;/P&gt;&lt;P&gt;&amp;gt; Can freescale guarantee the CLKO output for test only?&lt;/P&gt;&lt;P&gt;&amp;gt; Or can freescale guarantee the output for any usage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to your reply, 'test only' seems correct, right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2014 11:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335835#M45623</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-12-10T11:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL CLKO support range.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335836#M45624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes correct, main purpose is for test.&lt;/P&gt;&lt;P&gt;It also can be used for other purposes, provided&lt;/P&gt;&lt;P&gt;that one carefully design hard&amp;amp;software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2014 13:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335836#M45624</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-10T13:44:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL CLKO support range.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335837#M45625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I have been confused yet to understand whether other purpose is supported or not.&lt;/P&gt;&lt;P&gt;Which is right?&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;Support usage : test only&lt;/P&gt;&lt;P&gt;It can be used for other purpose even though it is not support.&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;Support usage : both test &amp;amp; other purpose&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Dec 2014 08:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335837#M45625</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-12-11T08:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL CLKO support range.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335838#M45626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Support usage : test only&lt;/P&gt;&lt;P&gt;It can be used for other purposes&lt;/P&gt;&lt;P&gt;provided that one carefully design hard&amp;amp;software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is one needs to have good knowledge of i.MX6 hardware and software,&lt;/P&gt;&lt;P&gt;then there will be no problems with its usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Dec 2014 08:33:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-CLKO-support-range/m-p/335838#M45626</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-11T08:33:09Z</dc:date>
    </item>
  </channel>
</rss>