<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What configuration is needed for QML to work? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147498#M456</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;A post by Pierre Vorraghen &amp;amp; Donald R Poole, Jr, suggests, that we need to include qtdeclarative, qtbase, qtxmlpatterns,&amp;nbsp;qtjsbackend, If I need to use the qml based designs from the qml sources made &amp;amp; ported to the target.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Is it that I should use, -qt-declarative -qt-base -qt-xmlpatterns -qt-jsbackend in ./configure arguments along with other conf. parameters.&lt;/P&gt;
&lt;P&gt;Please give me the proper pattern, as the above pattern[my trial] doesn't help me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2012 08:33:14 GMT</pubDate>
    <dc:creator>KrishnaPavan</dc:creator>
    <dc:date>2012-03-29T08:33:14Z</dc:date>
    <item>
      <title>What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147491#M449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone know how I should configure Qt so that QML will work?&amp;nbsp; I am using an i.MX28 with no X11 support and no hardware accelerated graphics.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Looking through the list of configurable components, I am unsure if webkit, javascript-jit, or script will make QML work (or maybe other features are necessary).&amp;nbsp; And I have been unable to find anything that specifically says what to configure.&amp;nbsp; I am trying to keep the Qt library as small as possible so I do not want to install features that are unnecessary for my platform.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Also, is it a mistake to try to use QML without hardware accelerated graphics?&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Thank you!&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;- Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2012 17:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147491#M449</guid>
      <dc:creator>Matt_ng9</dc:creator>
      <dc:date>2012-03-21T17:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147493#M451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Matt,&lt;/P&gt;
&lt;P&gt;Assuming you are building Qt-4.7+, by default the configure script will configure Qt with QML (as a release and debug library). &amp;nbsp;Note that the nomenclature changes from &lt;EM&gt;QML&lt;/EM&gt; to &lt;EM&gt;Declarative&lt;/EM&gt; within the context of Qt configuration. &amp;nbsp;So that's probably why you missed it the first time. &amp;nbsp;You can enable QML (delcarative) with the &lt;EM&gt;-declarative&lt;/EM&gt; option or disable it with &lt;EM&gt;-no-declarative&lt;/EM&gt; option.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;As for being a mistake to use QML without hardware accelerated graphics, I can't give you a confident answer. &amp;nbsp;Although, enabling hardware acceleration will definitely help, so I would enable it if you can.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2012 19:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147493#M451</guid>
      <dc:creator>DonaldR_PooleJr</dc:creator>
      <dc:date>2012-03-21T19:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147494#M452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the help Pierre and Donald!&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Sorry I forgot to mention, but I am dealing with 4.7.3, and the i.MX28 has no hardware accelerated graphics (it has alpha blending layers but no Qt support for that).&amp;nbsp; So I am stuck with the framebuffer.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;I built my Qt library with -no-declarative flag, so I will try with -declarative first, then try adding xml and js if it still does not work.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;- Matt&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2012 20:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147494#M452</guid>
      <dc:creator>Matt_ng9</dc:creator>
      <dc:date>2012-03-21T20:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147495#M453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;We are using declarative controls in Qt 4.7.1 on a imx233. It can get a bit choppy if you try to do a lot of animation control on the screen, i.e. transitions and wipes etc. But other than that its fine. Looks very good.&lt;/P&gt;
&lt;P&gt;We are using QML, XML and various image formats&lt;/P&gt;
&lt;P&gt;If it's any help the configure script we use is attached, FYI we are building statically which you may not want! There are a lot of unwritten dependencies in the Qt build that make it a pain to reduce the size of the build on a fine-grained basis.&lt;/P&gt;
&lt;P&gt;Good luck.&lt;/P&gt;
&lt;P&gt;Humphrey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2012 09:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147495#M453</guid>
      <dc:creator>hbucknell</dc:creator>
      <dc:date>2012-03-22T09:36:46Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147496#M454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;
&lt;P&gt;I have got a hello world program, and to run it on my PC, I have used qmlviewer.&lt;/P&gt;
&lt;P&gt;But, that application is not on my target rootfs.&lt;/P&gt;
&lt;P&gt;Then, Is it that "Enabling Qt Declarative, Will get me that application, so that I can run QML on my Target?&amp;nbsp; "&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Please Suggest!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Mar 2012 07:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147496#M454</guid>
      <dc:creator>KrishnaPavan</dc:creator>
      <dc:date>2012-03-26T07:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147497#M455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, enabling Qt Declarative (&lt;EM&gt;-delcarative&lt;/EM&gt; configure flag) in the configuration will build the declarative library and allow you to run your QML application on the target system.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Mar 2012 14:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147497#M455</guid>
      <dc:creator>DonaldR_PooleJr</dc:creator>
      <dc:date>2012-03-26T14:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147498#M456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;A post by Pierre Vorraghen &amp;amp; Donald R Poole, Jr, suggests, that we need to include qtdeclarative, qtbase, qtxmlpatterns,&amp;nbsp;qtjsbackend, If I need to use the qml based designs from the qml sources made &amp;amp; ported to the target.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Is it that I should use, -qt-declarative -qt-base -qt-xmlpatterns -qt-jsbackend in ./configure arguments along with other conf. parameters.&lt;/P&gt;
&lt;P&gt;Please give me the proper pattern, as the above pattern[my trial] doesn't help me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2012 08:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147498#M456</guid>
      <dc:creator>KrishnaPavan</dc:creator>
      <dc:date>2012-03-29T08:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147500#M458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;But, If we want to build embedded_linux, then we need to use qt-opensource-everywhere right?&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;+&amp;nbsp; -declarative ....... Build the declarative module. is what I have in my ./configure -help [ Thanks for the link @ Pierre].&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;But I could not get qmlviewer in my /bin in the Qt-Target-Directory.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Please tell me, How to get qmlviewer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2012 09:22:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147500#M458</guid>
      <dc:creator>KrishnaPavan</dc:creator>
      <dc:date>2012-03-29T09:22:06Z</dc:date>
    </item>
    <item>
      <title>Re: What configuration is needed for QML to work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147501#M459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Krishna,&lt;/P&gt;
&lt;P&gt;You actually don't need the qmlviewer on your target device. &amp;nbsp;You can simple cross-compile your QML app linking against ARM declarative module and execute the QML app just like any other executable. &amp;nbsp;If you really need the QML Viewer, then you well need to cross-compile the Qt4 or Qt5 SDK for the i.MX53 QSB. &amp;nbsp;I don't have much experience with cross-compiling the SDK, but I know it can and has been done (e.g. the Gumstix community has recipes for this).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Donald&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Mar 2012 16:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-configuration-is-needed-for-QML-to-work/m-p/147501#M459</guid>
      <dc:creator>DonaldR_PooleJr</dc:creator>
      <dc:date>2012-03-30T16:43:46Z</dc:date>
    </item>
  </channel>
</rss>