<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Simple Audio setup in Linux iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Simple-Audio-setup-in-Linux-iMX6/m-p/334761#M45446</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid not, just for quick reference please look at attached&lt;/P&gt;&lt;P&gt;documents Chapters Porting Audio Codecs to a Custom Board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Feb 2015 10:35:03 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-02-25T10:35:03Z</dc:date>
    <item>
      <title>Simple Audio setup in Linux iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simple-Audio-setup-in-Linux-iMX6/m-p/334760#M45445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a simple audio setup on my board. I have an external DAC+Amplifier that connects to iMX6 over I2S and to a speaker (Mono).&lt;/P&gt;&lt;P&gt;There are no controls for the 'codec' -- it just plays what is sent over I2S.&lt;/P&gt;&lt;P&gt;There's no headphone or microphone... just one output with no configuration options.&lt;/P&gt;&lt;P&gt;(iMX6 is I2S Master, for clocking)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use '&lt;EM&gt;simple-audio-card&lt;/EM&gt;' or something else to easily set up such a configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 20:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simple-Audio-setup-in-Linux-iMX6/m-p/334760#M45445</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2015-02-24T20:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: Simple Audio setup in Linux iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simple-Audio-setup-in-Linux-iMX6/m-p/334761#M45446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid not, just for quick reference please look at attached&lt;/P&gt;&lt;P&gt;documents Chapters Porting Audio Codecs to a Custom Board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 10:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simple-Audio-setup-in-Linux-iMX6/m-p/334761#M45446</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-02-25T10:35:03Z</dc:date>
    </item>
  </channel>
</rss>