<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Android Gingerbread Demo image can't work in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166221#M4543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to change the bootcmd_SD2 environment variable as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;setenv bootcmd_SD2 'mmc read&amp;nbsp;0 ${loadaddr} 0x800 0x2000;mmc read&amp;nbsp;0&amp;nbsp;${rd_loadaddr} 0x3000 0x300;bootm ${loadaddr} ${rd_loadaddr}'&lt;/P&gt;&lt;P&gt;This tells U-Boot to load the OS from the micro-SD card slot instead of the full-size SD card slot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Aug 2011 07:16:14 GMT</pubDate>
    <dc:creator>AlanLevy</dc:creator>
    <dc:date>2011-08-22T07:16:14Z</dc:date>
    <item>
      <title>Android Gingerbread Demo image can't work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166220#M4542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I used the QSB of "i.MX53-QSB-Android-Gingerbread-Release4.0" ,download the image by the "flash_prebuild_android.sh " in the folder "scripts".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Boot environment variables are set as follows(referenced the document "Adeneo i.MX53 Quick Start Board BSP for Android Gingerbread User Guide and Release Notes v4.0"):&lt;/P&gt;&lt;P&gt;&amp;nbsp; # setenv ethaddr 00:04:9f:01:b4:08&lt;BR /&gt;&amp;nbsp; # setenv fec_addr ${ethaddr}&lt;BR /&gt;&amp;nbsp; # setenv bootcmd ‘run bootcmd_SD1 bootcmd_SD2’&lt;BR /&gt;&amp;nbsp; # setenv bootcmd_SD1 'run bootargs_base bootargs_android'&lt;BR /&gt;&amp;nbsp; # setenv bootcmd_SD2 'mmc read 1 ${loadaddr} 0x800 0x2000;mmc read 1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ${rd_loadaddr} 0x3000 0x300;bootm ${loadaddr} ${rd_loadaddr}'&lt;BR /&gt;&amp;nbsp; # setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'&lt;BR /&gt;&amp;nbsp; # setenv vga ‘setenv bootargs ${bootargs} init=/init&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; androidboot.console=ttymxc0 di1_primary tve ip=dhcp’&lt;BR /&gt;&amp;nbsp; #setenv lcd ‘setenv bootargs ${bootargs} init=/init&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; androidboot.console=ttymxc0 di0_primary calibration ip=dhcp'&lt;BR /&gt;&amp;nbsp; # setenv bootargs_android ${lcd}&lt;BR /&gt;&amp;nbsp; # setenv loadaddr 0x70800000&lt;BR /&gt;&amp;nbsp; # setenv rd_loadaddr 0x70D00000&lt;BR /&gt;&amp;nbsp; # saveenv&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; But,the board can't run,and the log said:&lt;/P&gt;&lt;P&gt;&amp;nbsp; U-Boot 2009.08-00301-g3b48208-dirty (Jun 24 2011 - 12:48:27)&lt;/P&gt;&lt;P&gt;&amp;nbsp; CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX53 family 2.1V at 800 MHz&lt;BR /&gt;&amp;nbsp; mx53 pll1: 800MHz&lt;BR /&gt;&amp;nbsp; mx53 pll2: 400MHz&lt;BR /&gt;&amp;nbsp; mx53 pll3: 216MHz&lt;BR /&gt;&amp;nbsp; mx53 pll4: 455MHz&lt;BR /&gt;&amp;nbsp; ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 66666666Hz&lt;BR /&gt;&amp;nbsp; ipg per clock : 33333333Hz&lt;BR /&gt;&amp;nbsp; uart clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 66666666Hz&lt;BR /&gt;&amp;nbsp; cspi clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 54000000Hz&lt;BR /&gt;&amp;nbsp; ahb clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 133333333Hz&lt;BR /&gt;&amp;nbsp; axi_a clock&amp;nbsp;&amp;nbsp; : 400000000Hz&lt;BR /&gt;&amp;nbsp; axi_b clock&amp;nbsp;&amp;nbsp; : 200000000Hz&lt;BR /&gt;&amp;nbsp; emi_slow clock: 133333333Hz&lt;BR /&gt;&amp;nbsp; ddr clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 400000000Hz&lt;BR /&gt;&amp;nbsp; esdhc1 clock&amp;nbsp; : 80000000Hz&lt;BR /&gt;&amp;nbsp; esdhc2 clock&amp;nbsp; : 80000000Hz&lt;BR /&gt;&amp;nbsp; esdhc3 clock&amp;nbsp; : 80000000Hz&lt;BR /&gt;&amp;nbsp; esdhc4 clock&amp;nbsp; : 80000000Hz&lt;BR /&gt;&amp;nbsp; nfc clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 26666666Hz&lt;BR /&gt;&amp;nbsp; Board: MX53-LOCO 1.0&lt;BR /&gt;&amp;nbsp; Boot Reason: [POR]&lt;BR /&gt;&amp;nbsp; Boot Device: SD&lt;BR /&gt;&amp;nbsp; I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;&amp;nbsp; DRAM:&amp;nbsp;&amp;nbsp; 1 GB&lt;BR /&gt;&amp;nbsp; MMC:&amp;nbsp;&amp;nbsp; FSL_ESDHC: 0, FSL_ESDHC: 1&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&amp;nbsp; Card did not respond to voltage select!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&amp;nbsp; MMC init failed&lt;/SPAN&gt;&lt;BR /&gt;&amp;nbsp; In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;&amp;nbsp; Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;&amp;nbsp; Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;&amp;nbsp; Serial reinitilized!&lt;BR /&gt;&amp;nbsp; Checking for recovery command file...&lt;BR /&gt;&amp;nbsp; Net:&amp;nbsp;&amp;nbsp; got MAC address from IIM: 00:04:9f:01:b4:08&lt;BR /&gt;&amp;nbsp; FEC0&lt;BR /&gt;&amp;nbsp; MX53-LOCO U-Boot &amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; It stops here and doesn't go on.&lt;/P&gt;&lt;P&gt;&amp;nbsp; What's wrong?please your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Sorry for my English.&lt;/P&gt;&lt;P&gt;Thank!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Aug 2011 09:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166220#M4542</guid>
      <dc:creator>zhoujie</dc:creator>
      <dc:date>2011-08-20T09:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: Android Gingerbread Demo image can't work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166221#M4543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to change the bootcmd_SD2 environment variable as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;setenv bootcmd_SD2 'mmc read&amp;nbsp;0 ${loadaddr} 0x800 0x2000;mmc read&amp;nbsp;0&amp;nbsp;${rd_loadaddr} 0x3000 0x300;bootm ${loadaddr} ${rd_loadaddr}'&lt;/P&gt;&lt;P&gt;This tells U-Boot to load the OS from the micro-SD card slot instead of the full-size SD card slot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2011 07:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166221#M4543</guid>
      <dc:creator>AlanLevy</dc:creator>
      <dc:date>2011-08-22T07:16:14Z</dc:date>
    </item>
    <item>
      <title>Re: Android Gingerbread Demo image can't work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166222#M4544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, as I'm new, where should I change it (under which path should I find the file where to change this parameter)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried looking under src/kernel_imx , but I cannot find it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2011 08:39:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166222#M4544</guid>
      <dc:creator>MassimoPolizzi</dc:creator>
      <dc:date>2011-09-08T08:39:26Z</dc:date>
    </item>
    <item>
      <title>Re: Android Gingerbread Demo image can't work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166223#M4545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;setenv is done prior to loading the OS so at your prompt you type type the command above. There is a document for the U-Boot called uboot_mxc.fm in your docs directory&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2011 18:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Gingerbread-Demo-image-can-t-work/m-p/166223#M4545</guid>
      <dc:creator>RichardFelician</dc:creator>
      <dc:date>2011-09-08T18:11:54Z</dc:date>
    </item>
  </channel>
</rss>