<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic About the Wake on LAN sample source code for MX6DL-SABRE-SDP Linux BSP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-the-Wake-on-LAN-sample-source-code-for-MX6DL-SABRE-SDP/m-p/334113#M45328</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Our customer wants to make a system using i.MX6Solo and PF0100.&lt;BR /&gt;They are going to wake-up a system by an Ethernet.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have the following several questions.&lt;/P&gt;&lt;P&gt;1)&lt;BR /&gt;According to section "23.5.7.1 Sleep mode"(P.1132) of a reference manual, the following is explained.&lt;BR /&gt;"In addition, when the processor is in Stop mode, Sleep mode is entered, without affecting the ENETn_ECR register bits.&lt;/P&gt;&lt;P&gt;When a processor is Standby or Deep Sleep mode, can MAC enter a Sleep mode?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2)&lt;BR /&gt;They use LinuxBSP.&lt;BR /&gt;Is there a sample cord for a system to be waked-up by a Magic packet of Ethernet?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Dec 2014 07:13:30 GMT</pubDate>
    <dc:creator>yuuki</dc:creator>
    <dc:date>2014-12-09T07:13:30Z</dc:date>
    <item>
      <title>About the Wake on LAN sample source code for MX6DL-SABRE-SDP Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-the-Wake-on-LAN-sample-source-code-for-MX6DL-SABRE-SDP/m-p/334113#M45328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Our customer wants to make a system using i.MX6Solo and PF0100.&lt;BR /&gt;They are going to wake-up a system by an Ethernet.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have the following several questions.&lt;/P&gt;&lt;P&gt;1)&lt;BR /&gt;According to section "23.5.7.1 Sleep mode"(P.1132) of a reference manual, the following is explained.&lt;BR /&gt;"In addition, when the processor is in Stop mode, Sleep mode is entered, without affecting the ENETn_ECR register bits.&lt;/P&gt;&lt;P&gt;When a processor is Standby or Deep Sleep mode, can MAC enter a Sleep mode?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2)&lt;BR /&gt;They use LinuxBSP.&lt;BR /&gt;Is there a sample cord for a system to be waked-up by a Magic packet of Ethernet?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2014 07:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-the-Wake-on-LAN-sample-source-code-for-MX6DL-SABRE-SDP/m-p/334113#M45328</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2014-12-09T07:13:30Z</dc:date>
    </item>
    <item>
      <title>Re: About the Wake on LAN sample source code for MX6DL-SABRE-SDP Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-the-Wake-on-LAN-sample-source-code-for-MX6DL-SABRE-SDP/m-p/334114#M45329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi yuuki&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;official linux BSP does not support wake on lan, however&lt;/P&gt;&lt;P&gt;there is Community patch below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/360555"&gt;Wake on lan in mx6 sabresd board&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2014 07:44:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-the-Wake-on-LAN-sample-source-code-for-MX6DL-SABRE-SDP/m-p/334114#M45329</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-09T07:44:31Z</dc:date>
    </item>
  </channel>
</rss>