<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6 DDR_SEL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR-SEL/m-p/333995#M45306</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;In the i.MX6 reference manual [1] section &lt;SPAN style="color: #000000;"&gt;37.4.289 (IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET) it says the DDR_SEL field should be '11' for DDR3.&amp;nbsp; Value '00' is marked as reserved.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;Looking at the code for DRAM setup u-boot from the Freescale git repository[2], it sets the bits to '00' (reserved).&amp;nbsp; I also see this as the recommended setting in the DDR3 setup spread sheet[3].&amp;nbsp; Which value for those bits is the correct one?&lt;BR style="text-align: -webkit-auto;" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt; color: #000000;"&gt;[1] i.MX 6Solo/6DualLite Applications Processor Reference Manual&lt;BR /&gt;Document Number: IMX6SDLRM Rev. 1, 04/2013&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt;"&gt;[2] &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6qsabresd/mx6dl_4x_mt41j128.cfg?h=imx_v2013.04_3.10.17_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6qsabresd/mx6dl_4x_mt41j128.cfg?h=imx_v2013.04_3.10.17_1.0.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt;"&gt;[3] I.MX6DQSDL DDR3 Script Aid V0.10 &lt;/SPAN&gt;&lt;A href="https://community.nxp.com/docs/DOC-94917"&gt;https://community.nxp.com/docs/DOC-94917&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Oct 2014 17:25:33 GMT</pubDate>
    <dc:creator>andrewdyer</dc:creator>
    <dc:date>2014-10-17T17:25:33Z</dc:date>
    <item>
      <title>imx6 DDR_SEL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR-SEL/m-p/333995#M45306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;In the i.MX6 reference manual [1] section &lt;SPAN style="color: #000000;"&gt;37.4.289 (IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET) it says the DDR_SEL field should be '11' for DDR3.&amp;nbsp; Value '00' is marked as reserved.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;Looking at the code for DRAM setup u-boot from the Freescale git repository[2], it sets the bits to '00' (reserved).&amp;nbsp; I also see this as the recommended setting in the DDR3 setup spread sheet[3].&amp;nbsp; Which value for those bits is the correct one?&lt;BR style="text-align: -webkit-auto;" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt; color: #000000;"&gt;[1] i.MX 6Solo/6DualLite Applications Processor Reference Manual&lt;BR /&gt;Document Number: IMX6SDLRM Rev. 1, 04/2013&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt;"&gt;[2] &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6qsabresd/mx6dl_4x_mt41j128.cfg?h=imx_v2013.04_3.10.17_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6qsabresd/mx6dl_4x_mt41j128.cfg?h=imx_v2013.04_3.10.17_1.0.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt;"&gt;[3] I.MX6DQSDL DDR3 Script Aid V0.10 &lt;/SPAN&gt;&lt;A href="https://community.nxp.com/docs/DOC-94917"&gt;https://community.nxp.com/docs/DOC-94917&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Oct 2014 17:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR-SEL/m-p/333995#M45306</guid>
      <dc:creator>andrewdyer</dc:creator>
      <dc:date>2014-10-17T17:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 DDR_SEL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR-SEL/m-p/333996#M45307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Rev 2 version of the i.MX 6DQ Reference Manual correctly describes this register field as:&lt;/P&gt;&lt;P&gt;00&amp;nbsp; DDR3_LPDDR2 - DDR2 and LPDDR2 mode.&lt;BR /&gt;01&amp;nbsp; Reserved1 - Reserved&lt;/P&gt;&lt;P&gt;10&amp;nbsp; Reserved2 - Reserved&lt;/P&gt;&lt;P&gt;11&amp;nbsp; Reserved3 - Reserved&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A CQ ticket has been submitted to update the other Reference Manuals in the i.MX 6 familiy to read the same way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DRAM_RESET pin is not a true high speed pin. It is either low when the DDR is not in operation, or it is high once the DDR has been initialized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The correct setting for this pin is '00'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Oct 2014 20:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR-SEL/m-p/333996#M45307</guid>
      <dc:creator>TheAdmiral</dc:creator>
      <dc:date>2014-10-17T20:11:39Z</dc:date>
    </item>
  </channel>
</rss>