<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question, i.MX28 DISABLE_STEPPING bit</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-DISABLE-STEPPING-bit/m-p/333880#M45277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q1. If one desires to disable default stepping behavior, does one need to set DISABLE_STEPPING-bit every time TRG bit is changed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A1. No.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2. Change TRG then set DISABLE_STEPPING bit, Or, set DISABLE_STEPPING then change TRG?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A2. Set DISABLE_STEPPING then change TRG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3. Is it possible for internal DCDC converter to have incorrect voltage by incorrect procedure of setting DISABLE_STEPPING bit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A3. This is not a known issue.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Dec 2014 11:48:22 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2014-12-30T11:48:22Z</dc:date>
    <item>
      <title>Question, i.MX28 DISABLE_STEPPING bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-DISABLE-STEPPING-bit/m-p/333879#M45276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about the DISABLE_STEPPING bit in HW_POWER_VDDDCTRL register of i.MX28.&lt;/P&gt;&lt;P&gt;(1)&lt;/P&gt;&lt;P&gt;If one desires to disable default stepping behavior, does one need to set DISABLE_STEPPING-bit every time TRG bit is changed?&lt;/P&gt;&lt;P&gt;(2)&lt;/P&gt;&lt;P&gt;And please let me know the correct sequence on setting DISABLE_STEPPING bit.&lt;/P&gt;&lt;P&gt;Change TRG then set DISABLE_STEPPING bit, Or, set DISABLE_STEPPING then change TRG?&lt;/P&gt;&lt;P&gt;(3)&lt;/P&gt;&lt;P&gt;Is it possible for internal DCDC converter to have incorrect voltage by incorrect procedure of setting DISABLE_STEPPING bit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2014 04:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-DISABLE-STEPPING-bit/m-p/333879#M45276</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2014-12-09T04:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX28 DISABLE_STEPPING bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-DISABLE-STEPPING-bit/m-p/333880#M45277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q1. If one desires to disable default stepping behavior, does one need to set DISABLE_STEPPING-bit every time TRG bit is changed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A1. No.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2. Change TRG then set DISABLE_STEPPING bit, Or, set DISABLE_STEPPING then change TRG?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A2. Set DISABLE_STEPPING then change TRG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3. Is it possible for internal DCDC converter to have incorrect voltage by incorrect procedure of setting DISABLE_STEPPING bit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A3. This is not a known issue.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Dec 2014 11:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-DISABLE-STEPPING-bit/m-p/333880#M45277</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2014-12-30T11:48:22Z</dc:date>
    </item>
  </channel>
</rss>