<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: booting problem with U-boot on iMX6Q processor on custom board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/booting-problem-with-U-boot-on-iMX6Q-processor-on-custom-board/m-p/333475#M45166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for late...&lt;/P&gt;&lt;P&gt;Thanks a lot for reply,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;actually I tried as per your suggestion and also use new one SD card and boot up board but its not worked.&lt;/P&gt;&lt;P&gt;Board only detected serial flash (SF) after power ON and stop the prompt at that point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, Is there any other way to create SD card or directly flash u-boot into processor ??&lt;/P&gt;&lt;P&gt;And one more thing that I also tried to made SD card contain only u-boot.imx and made it by DD command as link suggested by you in reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So suggest any new way to bring up that custom board.&lt;/P&gt;&lt;P&gt;Waiting for your suggestion......&lt;/P&gt;&lt;P&gt;Reply soon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jaymin D&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Nov 2014 06:04:51 GMT</pubDate>
    <dc:creator>jaymind</dc:creator>
    <dc:date>2014-11-04T06:04:51Z</dc:date>
    <item>
      <title>booting problem with U-boot on iMX6Q processor on custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/booting-problem-with-U-boot-on-iMX6Q-processor-on-custom-board/m-p/333473#M45164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have custom board name as 'camaro' with iMX6 Quad processor.&lt;BR /&gt;I faced &lt;SPAN class="sac"&gt;a problem&lt;/SPAN&gt; when I update my u-boot from &lt;SPAN class="sac"&gt;mmc&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apply &lt;STRONG&gt;'run &lt;/STRONG&gt;&lt;CODE class="shell plain"&gt;&lt;STRONG&gt;upgrade_uboot&lt;/STRONG&gt;' into uboot prompt &lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE class="shell plain"&gt;then after I &lt;SPAN class="sac"&gt;didn't get&lt;/SPAN&gt; any prompt to run &lt;SPAN class="sac"&gt;the next command&lt;/SPAN&gt;...&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE class="shell plain"&gt;&lt;/CODE&gt;then I restarted my board but I didn't get any prompt.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I included some outputs below&lt;/P&gt;&lt;P&gt;I'm not really sure what the problem could be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2013.07 (Jul 24 2014 - 14:51:00)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.2 at 792 MHz&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: MX6Q-Camaro&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 1 GiB&lt;/P&gt;&lt;P&gt;MMC:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2013.07 (Jul 24 2014 - 14:51:00)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.2 at 792 MHz&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: MX6Q-Camaro&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 1 GiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/P&gt;&lt;P&gt;SF: Detected S25FL512SA with page size 64 KiB, total 64 MiB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;somehow is there any &lt;SPAN class="sac"&gt;possibilities&lt;/SPAN&gt; to restore or reset u-boot into its default &lt;SPAN class="sac"&gt;state&lt;/SPAN&gt; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Oct 2014 14:18:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/booting-problem-with-U-boot-on-iMX6Q-processor-on-custom-board/m-p/333473#M45164</guid>
      <dc:creator>jaymind</dc:creator>
      <dc:date>2014-10-17T14:18:52Z</dc:date>
    </item>
    <item>
      <title>Re: booting problem with U-boot on iMX6Q processor on custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/booting-problem-with-U-boot-on-iMX6Q-processor-on-custom-board/m-p/333474#M45165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaymin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;probably "upgrade.." is not implemented in that uboot.&lt;/P&gt;&lt;P&gt;One can try to write sd with sudo dd..&amp;nbsp; as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94989"&gt;Task #4 - Deploy and test&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Oct 2014 07:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/booting-problem-with-U-boot-on-iMX6Q-processor-on-custom-board/m-p/333474#M45165</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-18T07:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: booting problem with U-boot on iMX6Q processor on custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/booting-problem-with-U-boot-on-iMX6Q-processor-on-custom-board/m-p/333475#M45166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for late...&lt;/P&gt;&lt;P&gt;Thanks a lot for reply,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;actually I tried as per your suggestion and also use new one SD card and boot up board but its not worked.&lt;/P&gt;&lt;P&gt;Board only detected serial flash (SF) after power ON and stop the prompt at that point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, Is there any other way to create SD card or directly flash u-boot into processor ??&lt;/P&gt;&lt;P&gt;And one more thing that I also tried to made SD card contain only u-boot.imx and made it by DD command as link suggested by you in reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So suggest any new way to bring up that custom board.&lt;/P&gt;&lt;P&gt;Waiting for your suggestion......&lt;/P&gt;&lt;P&gt;Reply soon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jaymin D&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Nov 2014 06:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/booting-problem-with-U-boot-on-iMX6Q-processor-on-custom-board/m-p/333475#M45166</guid>
      <dc:creator>jaymind</dc:creator>
      <dc:date>2014-11-04T06:04:51Z</dc:date>
    </item>
  </channel>
</rss>