<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Custom IMX6Q Hardware Board Bringup Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX6Q-Hardware-Board-Bringup-Issue/m-p/333353#M45143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom IMX6Q based hardware. I have checked the power supplies and sequencing of these power supplies and that seems to be okay. I have measured various CAP voltages and they are also fine except VDDUSB_CAP which is 2.7V instead of 3V. Is this a problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been trying to boot in Serial downloader mode by setting the boot mode pins as required but the Host machine doesn't detect my&amp;nbsp; board as HID complaint device as explained in DDR Tester User manual. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone suggest some ways in order to make sure that the USB OTG Serial downloader works. Any suggestion is welcome.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Raj Nikumbh &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Sep 2014 13:43:11 GMT</pubDate>
    <dc:creator>rajniks</dc:creator>
    <dc:date>2014-09-02T13:43:11Z</dc:date>
    <item>
      <title>Custom IMX6Q Hardware Board Bringup Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX6Q-Hardware-Board-Bringup-Issue/m-p/333353#M45143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom IMX6Q based hardware. I have checked the power supplies and sequencing of these power supplies and that seems to be okay. I have measured various CAP voltages and they are also fine except VDDUSB_CAP which is 2.7V instead of 3V. Is this a problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been trying to boot in Serial downloader mode by setting the boot mode pins as required but the Host machine doesn't detect my&amp;nbsp; board as HID complaint device as explained in DDR Tester User manual. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone suggest some ways in order to make sure that the USB OTG Serial downloader works. Any suggestion is welcome.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Raj Nikumbh &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Sep 2014 13:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX6Q-Hardware-Board-Bringup-Issue/m-p/333353#M45143</guid>
      <dc:creator>rajniks</dc:creator>
      <dc:date>2014-09-02T13:43:11Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX6Q Hardware Board Bringup Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX6Q-Hardware-Board-Bringup-Issue/m-p/333354#M45144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can try to test processor with SDK (one can run it with jtag)&lt;/P&gt;&lt;P&gt;and test USB interface&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Bare-metal SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and check all items given in Chapter 2 Design Checklist&lt;/P&gt;&lt;P&gt;Chapter 8 Avoiding Board Bring-up Problems&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf?fasp=1&amp;amp;WT_TYPE=Users%20Guides&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQ6SDLHDG&lt;/A&gt;&amp;nbsp; IMX6DQ6SDLHDG, Hardware Development Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Sep 2014 15:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX6Q-Hardware-Board-Bringup-Issue/m-p/333354#M45144</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-02T15:09:37Z</dc:date>
    </item>
  </channel>
</rss>